<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: DMA max size</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-max-size/m-p/523099#M5735</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Mon Apr 28 13:08:53 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1KByte is very small. The LPC1769 can easily transfer a buffer of that size in a single LLI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The transfer-size is 12-bit, which means 4096 units, where a unit can be a byte, halfword or word.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That means: Your maximum transfer size would be 4096 if you're using bytes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-But as you can make a Linked List, there's no real limit to how many bytes you can transfer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See UM10360, section 31.6.5 "Scatter/gather" for more information on Linked List Items (LLI).&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:57:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:57:57Z</dc:date>
    <item>
      <title>DMA max size</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-max-size/m-p/523098#M5734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by guillaumeL on Mon Apr 28 11:49:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; I'm working with an LPC1769 and I use a DMA to transfert data from SPI to memory. I have a question concerning the maximum data size I can allocate for the DMA transfert. Is it limited or I can allocate a buffer of 1kbyte to transfer data?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Guillaume&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-max-size/m-p/523098#M5734</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:57Z</dc:date>
    </item>
    <item>
      <title>Re: DMA max size</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-max-size/m-p/523099#M5735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Mon Apr 28 13:08:53 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1KByte is very small. The LPC1769 can easily transfer a buffer of that size in a single LLI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The transfer-size is 12-bit, which means 4096 units, where a unit can be a byte, halfword or word.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That means: Your maximum transfer size would be 4096 if you're using bytes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-But as you can make a Linked List, there's no real limit to how many bytes you can transfer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See UM10360, section 31.6.5 "Scatter/gather" for more information on Linked List Items (LLI).&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-max-size/m-p/523099#M5735</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:57Z</dc:date>
    </item>
  </channel>
</rss>