<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to read LPC4317 register via IFC bus in u-boot (LS1021A ) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2002835#M57321</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with ls1021a custom board, which is having LPC4317 connected via IFC bus, I want to read the LPC4317 status , is their any command or other way to read the register in u-boot, please suggest me to get this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Saravanan S&lt;/P&gt;</description>
    <pubDate>Wed, 27 Nov 2024 11:34:00 GMT</pubDate>
    <dc:creator>Saravanans1</dc:creator>
    <dc:date>2024-11-27T11:34:00Z</dc:date>
    <item>
      <title>How to read LPC4317 register via IFC bus in u-boot (LS1021A )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2002835#M57321</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with ls1021a custom board, which is having LPC4317 connected via IFC bus, I want to read the LPC4317 status , is their any command or other way to read the register in u-boot, please suggest me to get this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Saravanan S&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 11:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2002835#M57321</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2024-11-27T11:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: How to read LPC4317 register via IFC bus in u-boot (LS1021A )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2007320#M57340</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can read the registers in u-boot with the md command:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/u-boot/u-boot/blob/master/doc/usage/cmd/md.rst" target="_blank"&gt;https://github.com/u-boot/u-boot/blob/master/doc/usage/cmd/md.rst&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In this case you have write the md command and the address of the register, for example in the&amp;nbsp;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=TWR-LS1021ARM" target="_self"&gt;TWR-LS1021A&lt;/A&gt; there is a CPLD connected to the IFC, you can review it as reference.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 17:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2007320#M57340</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-12-04T17:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to read LPC4317 register via IFC bus in u-boot (LS1021A )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2008135#M57353</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;Thanks for the information. Could please provide the LPC4312 status read and write register details through LS1021A?</description>
      <pubDate>Thu, 05 Dec 2024 11:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2008135#M57353</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2024-12-05T11:08:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to read LPC4317 register via IFC bus in u-boot (LS1021A )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2008612#M57359</link>
      <description>&lt;P&gt;There isn't any predefined read and write register (we don't have any example with &lt;SPAN&gt;LPC4312 and ls1021a together)&lt;/SPAN&gt;, from the side of the ls1021a it could be the address assigned either in IFC region 1 or region 2,&amp;nbsp; chip-selects, for more information you can refer to the LS1021ARM&amp;nbsp;Chapter 24 Integrated Flash Controller (IFC).&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 00:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2008612#M57359</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-12-06T00:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to read LPC4317 register via IFC bus in u-boot (LS1021A )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2008786#M57360</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;Thank you. Additionally, we require more details. For a 100 MHz system clock(LS1021A), is it possible to configure the DDR IFC clock to 192 MHz? If so, please provide the necessary information.</description>
      <pubDate>Fri, 06 Dec 2024 04:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-read-LPC4317-register-via-IFC-bus-in-u-boot-LS1021A/m-p/2008786#M57360</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2024-12-06T04:21:43Z</dc:date>
    </item>
  </channel>
</rss>