<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Target Reset Pattern</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Target-Reset-Pattern/m-p/2000807#M57306</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239137"&gt;@lb_h&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.&lt;/P&gt;
&lt;P&gt;The T-bit is typically calculated automatically by the hardware based on the I3C command.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
    <pubDate>Mon, 25 Nov 2024 07:42:39 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-11-25T07:42:39Z</dc:date>
    <item>
      <title>Target Reset Pattern</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Target-Reset-Pattern/m-p/1998675#M57299</link>
      <description>&lt;P&gt;Hello,all&lt;/P&gt;&lt;P&gt;Can the I3C module of the LPC55xx family of chips send a "Target Reset Pattern" through a configuration register?Whether the T-bit of the I3C command is automatically calculated by the hardware or can be configured by software.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Nov 2024 08:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Target-Reset-Pattern/m-p/1998675#M57299</guid>
      <dc:creator>lb_h</dc:creator>
      <dc:date>2024-11-21T08:16:00Z</dc:date>
    </item>
    <item>
      <title>Re: Target Reset Pattern</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Target-Reset-Pattern/m-p/2000807#M57306</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239137"&gt;@lb_h&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.&lt;/P&gt;
&lt;P&gt;The T-bit is typically calculated automatically by the hardware based on the I3C command.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 07:42:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Target-Reset-Pattern/m-p/2000807#M57306</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-11-25T07:42:39Z</dc:date>
    </item>
  </channel>
</rss>