<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC4337 and LCD TFT</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1982933#M57163</link>
    <description>&lt;P&gt;Thanks a lot for your answer. I have just bought the MIMIXRT1170_EVKB&amp;nbsp; , and the 5,5" display.&lt;/P&gt;&lt;P&gt;Now i am redy to play with these new toys..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nico&lt;/P&gt;</description>
    <pubDate>Mon, 28 Oct 2024 11:30:01 GMT</pubDate>
    <dc:creator>nicomarconi</dc:creator>
    <dc:date>2024-10-28T11:30:01Z</dc:date>
    <item>
      <title>LPC4337 and LCD TFT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1974112#M57061</link>
      <description>&lt;P&gt;Hi, i have used a LPC4337 bosrd based in a course i did a month ago, and i am very interested in use it in a project with a 10" touchscreen LCD TFT. It is possible to connect this kind of LCD to the LPC4337?&lt;/P&gt;&lt;P&gt;It is possible to use any graphic tool with the LPC4337.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case it is not possible , what&amp;nbsp; minimal and chipest microcontroller would you suggest me to use for LCD TFT 10" project?&lt;/P&gt;&lt;P&gt;Thanks a lot for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nicolás Marconi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 09:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1974112#M57061</guid>
      <dc:creator>nicomarconi</dc:creator>
      <dc:date>2024-10-15T09:11:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 and LCD TFT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1975059#M57075</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Because the LPC4437 has LCD interface and I2C interface, it is okay to connect LCD with touch screen, but you have to check if the board has interface with LCD.&lt;/P&gt;
&lt;P&gt;BTW, the LPC4437 is very old.&lt;/P&gt;
&lt;P&gt;If you are interested in the LCD display, pls try the GUI Guider.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/gui-guider:GUI-GUIDER" target="_blank"&gt;https://www.nxp.com/design/design-center/software/development-software/gui-guider:GUI-GUIDER&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For example, order:&lt;/P&gt;
&lt;P&gt;micro controller board:FRDM-MCXN947&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/frdm-development-board-for-mcx-n94-n54-mcus:FRDM-MCXN947" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/frdm-development-board-for-mcx-n94-n54-mcus:FRDM-MCXN947&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;LCD:3.5” 480x320 IPS TFT LCD Module&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/3-5-480x320-ips-tft-lcd-module:LCD-PAR-S035" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/3-5-480x320-ips-tft-lcd-module:LCD-PAR-S035&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I attach the pic of connection.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 09:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1975059#M57075</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-10-16T09:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 and LCD TFT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1982933#M57163</link>
      <description>&lt;P&gt;Thanks a lot for your answer. I have just bought the MIMIXRT1170_EVKB&amp;nbsp; , and the 5,5" display.&lt;/P&gt;&lt;P&gt;Now i am redy to play with these new toys..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nico&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 11:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-and-LCD-TFT/m-p/1982933#M57163</guid>
      <dc:creator>nicomarconi</dc:creator>
      <dc:date>2024-10-28T11:30:01Z</dc:date>
    </item>
  </channel>
</rss>