<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: HomePlug Green PHY communication via power line</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1981023#M57144</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233050"&gt;@JasonTseng&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The type of signal you would measure on the power line will typically depend on the modulation scheme used (such as OFDM, BPSK, QPSK). You can expect:&lt;BR /&gt;• Modulated RF signal: Typically, in the frequency range of tens to hundreds of kilohertz, or even up to a few megahertz, depending on the standard used.&lt;BR /&gt;• Amplitude or phase shifts: This depends on the specific modulation being used, such as phase-shift keying (PSK) or amplitude modulation.&lt;BR /&gt;• Noise: Power lines are a noisy environment, so you might see noise superimposed on the modulated signal.&lt;BR /&gt;You can measure this signal using an oscilloscope or a spectrum analyzer connected to the power line via an appropriate coupling circuit.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
    <pubDate>Thu, 24 Oct 2024 08:18:32 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-10-24T08:18:32Z</dc:date>
    <item>
      <title>HomePlug Green PHY communication via power line</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1978710#M57124</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;By using nxp LPC and connect to QCA7000, it can transmitting and receiving data over the power line.&lt;BR /&gt;Now my setup is LPC as a master in the SPI protocol, with the QCA7000 acting as a slave.&amp;nbsp;I am able to read/write qca register from LPC side. Next step is Powerline Communication.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Question: If start to transmit&amp;nbsp;data to power line, what kind of signal can be measured?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 02:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1978710#M57124</guid>
      <dc:creator>JasonTseng</dc:creator>
      <dc:date>2024-10-22T02:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: HomePlug Green PHY communication via power line</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1981023#M57144</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233050"&gt;@JasonTseng&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The type of signal you would measure on the power line will typically depend on the modulation scheme used (such as OFDM, BPSK, QPSK). You can expect:&lt;BR /&gt;• Modulated RF signal: Typically, in the frequency range of tens to hundreds of kilohertz, or even up to a few megahertz, depending on the standard used.&lt;BR /&gt;• Amplitude or phase shifts: This depends on the specific modulation being used, such as phase-shift keying (PSK) or amplitude modulation.&lt;BR /&gt;• Noise: Power lines are a noisy environment, so you might see noise superimposed on the modulated signal.&lt;BR /&gt;You can measure this signal using an oscilloscope or a spectrum analyzer connected to the power line via an appropriate coupling circuit.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 08:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1981023#M57144</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-10-24T08:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: HomePlug Green PHY communication via power line</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1981273#M57147</link>
      <description>&lt;P&gt;Hello Hang,&lt;/P&gt;
&lt;P&gt;Thanks for the response.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on the QCA's datasheet, it uses OFDM mode for communication.&lt;/P&gt;
&lt;P&gt;To measure OFDM signal using an oscilloscope connect to power line&lt;/P&gt;
&lt;P&gt;if we want to get data payload, should we measure it before or after PLC coupling?&lt;/P&gt;
&lt;P&gt;ps: I also check with ChatGPT but don't get good answer.&lt;/P&gt;
&lt;P&gt;Can you please help check with HW engineer?&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 13:09:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1981273#M57147</guid>
      <dc:creator>JasonTsengSG</dc:creator>
      <dc:date>2024-10-24T13:09:01Z</dc:date>
    </item>
    <item>
      <title>Re: HomePlug Green PHY communication via power line</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1984670#M57183</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239944"&gt;@JasonTsengSG&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;The QCA7000 is a chip introduced by Qualcomm.&lt;/P&gt;
&lt;P&gt;I think you should contact Qualcomm for instructions.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 10:27:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HomePlug-Green-PHY-communication-via-power-line/m-p/1984670#M57183</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-10-30T10:27:37Z</dc:date>
    </item>
  </channel>
</rss>