<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Identification of MCU_Link in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Identification-of-MCU-Link/m-p/1980305#M57135</link>
    <description>&lt;P&gt;Hi, I am trying to add a defined name to a mcu_link device, so I can connect to it instead of using its serial number.&lt;/P&gt;&lt;P&gt;I've followed the steps metioned in Readme.txt of mcu-link installer folder of LinkServer_24.9.75 regarding&amp;nbsp;device_vendor,&amp;nbsp;device_name, board_vendor, board_name. However none of these data can be seen with openocd or pyocd&lt;/P&gt;&lt;P&gt;Is there a way how I can modify the serial number?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Wed, 23 Oct 2024 14:51:49 GMT</pubDate>
    <dc:creator>bm31416</dc:creator>
    <dc:date>2024-10-23T14:51:49Z</dc:date>
    <item>
      <title>Identification of MCU_Link</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Identification-of-MCU-Link/m-p/1980305#M57135</link>
      <description>&lt;P&gt;Hi, I am trying to add a defined name to a mcu_link device, so I can connect to it instead of using its serial number.&lt;/P&gt;&lt;P&gt;I've followed the steps metioned in Readme.txt of mcu-link installer folder of LinkServer_24.9.75 regarding&amp;nbsp;device_vendor,&amp;nbsp;device_name, board_vendor, board_name. However none of these data can be seen with openocd or pyocd&lt;/P&gt;&lt;P&gt;Is there a way how I can modify the serial number?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 14:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Identification-of-MCU-Link/m-p/1980305#M57135</guid>
      <dc:creator>bm31416</dc:creator>
      <dc:date>2024-10-23T14:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: Identification of MCU_Link</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Identification-of-MCU-Link/m-p/1982575#M57158</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234089"&gt;@bm31416&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You cannot directly modify the serial number of a MCU-Link device, as the serial number is typically programmed into the hardware and is not designed to be changed. However, you can set a custom defined name for your MCU-Link device for easier identification without relying on the serial number.&lt;/P&gt;
&lt;P&gt;Ensure that you have properly modified the configuration files as mentioned in the Readme.txt file. Specifically:&lt;BR /&gt;Add your MCU-Link device’s details to the correct configuration file&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Ensure that the custom device_vendor, device_name, board_vendor, and board_name fields are entered correctly and match the syntax required by the configuration files.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 02:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Identification-of-MCU-Link/m-p/1982575#M57158</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-10-28T02:38:43Z</dc:date>
    </item>
  </channel>
</rss>