<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S69 USB fs host causes issues with ADC0 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1977432#M57108</link>
    <description>&lt;P&gt;Hello, my apologize for the delay response, we are experiencing a backlog, I reviewed your question and for this custom application I recommend review this document and thread.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12358.pdf" target="_blank"&gt;LPC55xx/LPC55Sxx Dual-Core Debug in MCUXpresso (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-Dual-Core-Best-Practice/td-p/946035" target="_blank"&gt;Solved: LPC55S6x Dual Core Best Practice - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Fri, 18 Oct 2024 21:57:19 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2024-10-18T21:57:19Z</dc:date>
    <item>
      <title>LPC55S69 USB fs host causes issues with ADC0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1976116#M57092</link>
      <description>&lt;P&gt;I'm using ADC0 with interrupts on CPU0 which works good, but when i enable USB FS Host on CPU1 i get random crashes on CPU0.&lt;/P&gt;&lt;P&gt;What happens is that the ADC0 irq is triggered but the fifo is empty.&lt;/P&gt;&lt;P&gt;It seems like it's a spurious irq but if the irq is just ignored there will be no additional irq that signals that data is available on in the fifo.&lt;/P&gt;&lt;P&gt;CPU0 runs in secure mode and CPU1 uses the unsecured memory space.&lt;BR /&gt;Could there be an issue with using USB-FS host and ADC0 from different cores?&lt;/P&gt;&lt;P&gt;I see that both are connected to the same AHB bus and both are also quite close in the memory map.&lt;/P&gt;&lt;P&gt;Regards, Johan&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 13:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1976116#M57092</guid>
      <dc:creator>johan_carlsson</dc:creator>
      <dc:date>2024-10-17T13:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 USB fs host causes issues with ADC0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1976384#M57098</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting our case, I will review your case, when I have more information, I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 20:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1976384#M57098</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-10-17T20:07:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 USB fs host causes issues with ADC0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1977432#M57108</link>
      <description>&lt;P&gt;Hello, my apologize for the delay response, we are experiencing a backlog, I reviewed your question and for this custom application I recommend review this document and thread.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12358.pdf" target="_blank"&gt;LPC55xx/LPC55Sxx Dual-Core Debug in MCUXpresso (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-Dual-Core-Best-Practice/td-p/946035" target="_blank"&gt;Solved: LPC55S6x Dual Core Best Practice - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 21:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-fs-host-causes-issues-with-ADC0/m-p/1977432#M57108</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-10-18T21:57:19Z</dc:date>
    </item>
  </channel>
</rss>