<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB0 FS Host Controller with FRO_HF clock.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-FS-Host-Controller-with-FRO-HF-clock/m-p/1966938#M56954</link>
    <description>&lt;P&gt;The documentation is&amp;nbsp;ambiguous in regard to if it's possible to use the FRO_HF clock when using the USB0 Full-speed Host Controller.&lt;/P&gt;&lt;P&gt;UM11126:&amp;nbsp;Table 37.&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;The currently selected FRO_192 high speed output at 96 MHz. FRO_HF clock is the output of the FRO_192 divided by 2 (96 MHz). Note that this clock can only be used for USB device and is not reliable for USB host timing requirements of the data signaling rate&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;AN13449:&amp;nbsp;4. Hardware design&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;When using FS USB host, HS USB host/device, external crystal must be connected.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;UM11126: 42.5.&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;Clock: To have the full-speed USB operating, select either the PLL1, or USB PLL, or FRO clock output as the USB0 clock and the clock must be 48 MHz&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The text above seems incorrect there is no USB PLL in the full-speed controller, it can also be used with PLL0. It does however state that the FRO clock can be used.&lt;/P&gt;&lt;P&gt;Is it recommended to use the FRO_HF clock with the USB0 Full-Speed Host controller?&lt;/P&gt;&lt;P&gt;Regards, Johan&lt;/P&gt;</description>
    <pubDate>Fri, 04 Oct 2024 13:16:52 GMT</pubDate>
    <dc:creator>johan_carlsson</dc:creator>
    <dc:date>2024-10-04T13:16:52Z</dc:date>
    <item>
      <title>USB0 FS Host Controller with FRO_HF clock.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-FS-Host-Controller-with-FRO-HF-clock/m-p/1966938#M56954</link>
      <description>&lt;P&gt;The documentation is&amp;nbsp;ambiguous in regard to if it's possible to use the FRO_HF clock when using the USB0 Full-speed Host Controller.&lt;/P&gt;&lt;P&gt;UM11126:&amp;nbsp;Table 37.&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;The currently selected FRO_192 high speed output at 96 MHz. FRO_HF clock is the output of the FRO_192 divided by 2 (96 MHz). Note that this clock can only be used for USB device and is not reliable for USB host timing requirements of the data signaling rate&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;AN13449:&amp;nbsp;4. Hardware design&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;When using FS USB host, HS USB host/device, external crystal must be connected.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;UM11126: 42.5.&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;Clock: To have the full-speed USB operating, select either the PLL1, or USB PLL, or FRO clock output as the USB0 clock and the clock must be 48 MHz&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The text above seems incorrect there is no USB PLL in the full-speed controller, it can also be used with PLL0. It does however state that the FRO clock can be used.&lt;/P&gt;&lt;P&gt;Is it recommended to use the FRO_HF clock with the USB0 Full-Speed Host controller?&lt;/P&gt;&lt;P&gt;Regards, Johan&lt;/P&gt;</description>
      <pubDate>Fri, 04 Oct 2024 13:16:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-FS-Host-Controller-with-FRO-HF-clock/m-p/1966938#M56954</guid>
      <dc:creator>johan_carlsson</dc:creator>
      <dc:date>2024-10-04T13:16:52Z</dc:date>
    </item>
    <item>
      <title>Re: USB0 FS Host Controller with FRO_HF clock.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-FS-Host-Controller-with-FRO-HF-clock/m-p/1970312#M56992</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/109785"&gt;@johan_carlsson&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The FRO_HF is not recommended for USB host because of the +/- 2% accuracy on the FRO (temperature/process/pcb/etc), result may vary. The FRO_HF is recommended in the implementation of a crystal-less FS USB device like in the example of the technical note TN00063.&lt;/P&gt;
&lt;P&gt;Since there is no option of crystal-less USB host it is mention on the hardware design that if you want to implement a FS USB host it would be required that the external crystal is connected.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 19:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-FS-Host-Controller-with-FRO-HF-clock/m-p/1970312#M56992</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2024-10-09T19:29:53Z</dc:date>
    </item>
  </channel>
</rss>