<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic - LPC5502 - can not trigger an SPI DMA transfer from CTimer0 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5502-can-not-trigger-an-SPI-DMA-transfer-from-CTimer0/m-p/1963751#M56929</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;I am a beginner with NXP MCUs.&amp;nbsp;I have a task that I cannot solve.&lt;/P&gt;&lt;P&gt;So, I want to configure &lt;STRONG&gt;CTimer0 Match0&lt;/STRONG&gt; to trigger the &lt;STRONG&gt;DMA&lt;/STRONG&gt; to transfer data over &lt;STRONG&gt;SPI&lt;/STRONG&gt; every 100 microseconds. From the user manual, as far as I can understand, this should be possible. However, I can't achieve it. Could someone create a simple project that does this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;kind regards&lt;/P&gt;</description>
    <pubDate>Fri, 27 Sep 2024 21:06:05 GMT</pubDate>
    <dc:creator>nico_2451</dc:creator>
    <dc:date>2024-09-27T21:06:05Z</dc:date>
    <item>
      <title>- LPC5502 - can not trigger an SPI DMA transfer from CTimer0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5502-can-not-trigger-an-SPI-DMA-transfer-from-CTimer0/m-p/1963751#M56929</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I am a beginner with NXP MCUs.&amp;nbsp;I have a task that I cannot solve.&lt;/P&gt;&lt;P&gt;So, I want to configure &lt;STRONG&gt;CTimer0 Match0&lt;/STRONG&gt; to trigger the &lt;STRONG&gt;DMA&lt;/STRONG&gt; to transfer data over &lt;STRONG&gt;SPI&lt;/STRONG&gt; every 100 microseconds. From the user manual, as far as I can understand, this should be possible. However, I can't achieve it. Could someone create a simple project that does this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;kind regards&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 21:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5502-can-not-trigger-an-SPI-DMA-transfer-from-CTimer0/m-p/1963751#M56929</guid>
      <dc:creator>nico_2451</dc:creator>
      <dc:date>2024-09-27T21:06:05Z</dc:date>
    </item>
    <item>
      <title>Re: - LPC5502 - can not trigger an SPI DMA transfer from CTimer0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5502-can-not-trigger-an-SPI-DMA-transfer-from-CTimer0/m-p/1964002#M56930</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241222"&gt;@nico_2451&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is a demo about SPI+DMA ''spi_dma" under LPC5506 SDK, it uses software trigger.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1727601661444.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/301834i317A52D012BCFDB0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1727601661444.png" alt="Alice_Yang_0-1727601661444.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can add Ctimer MATCH trigger based on it. About CTIMER&amp;nbsp; trigger SPI, you can refer to:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/DMA-triggering-function-Demo-for-LPC55xx-From-CTimer0-match0/ta-p/1468144" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/DMA-triggering-function-Demo-for-LPC55xx-From-CTimer0-match0/ta-p/1468144&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/CTIMER-DMA-requests-triggers-pacing-the-transfers/m-p/1088948" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/CTIMER-DMA-requests-triggers-pacing-the-transfers/m-p/1088948&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Sun, 29 Sep 2024 09:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5502-can-not-trigger-an-SPI-DMA-transfer-from-CTimer0/m-p/1964002#M56930</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-09-29T09:21:24Z</dc:date>
    </item>
  </channel>
</rss>