<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S26 PIO0_5 FC4_RXD use, ISP disable</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1963922#M56925</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167127"&gt;@alfredocyberhom&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;The problem arises because the boot mode selection (via PIO0_5 pin) takes precedence during reset, which causes the processor to jump to the ISP if the pin is low.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;To work around this issue, you can prevent the processor from entering the ISP mode by ensuring the state of PIO0_5 is high during reset. Since PIO0_5 is being used as a UART4 receiver (FC4_RXD), you have a couple of options:&lt;BR /&gt;You can add an external pull-up resistor (e.g., 10kΩ to 3.3V) to the PIO0_5 pin. This will ensure that PIO0_5 is high during reset, preventing the processor from entering ISP mode.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Hang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 29 Sep 2024 06:20:36 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-09-29T06:20:36Z</dc:date>
    <item>
      <title>LPC55S26 PIO0_5 FC4_RXD use, ISP disable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1960027#M56901</link>
      <description>&lt;P&gt;Hello, I'm working with a LPC55S26. I use the PIO0_5 pin as a UART4 receiver (FC4_RXD). The problem is that if this pin is low during reset (receiving data) it jumps to the ISP and my program doesn't start. Is there a way to disable the ISP function and make the pin work only as a UART4 receiver? I tried to write 0x70 in BOOT_CFG (0x9E400) but this didn't work.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 15:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1960027#M56901</guid>
      <dc:creator>alfredocyberhom</dc:creator>
      <dc:date>2024-09-23T15:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S26 PIO0_5 FC4_RXD use, ISP disable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1962360#M56911</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167127"&gt;@alfredocyberhom&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you try to read the CMPA,&amp;nbsp;Check if the writing is successful.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HangZhang_0-1727333121721.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/301359iE2367950DB01AD13/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HangZhang_0-1727333121721.png" alt="HangZhang_0-1727333121721.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HangZhang_1-1727333188405.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/301363i8DF17CF65853822F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HangZhang_1-1727333188405.png" alt="HangZhang_1-1727333188405.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 06:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1962360#M56911</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-09-26T06:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S26 PIO0_5 FC4_RXD use, ISP disable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1962695#M56915</link>
      <description>&lt;P&gt;I prepared the program image for the Cyclone (from PEMicro), setting bits 4-6 of BOOT_CFG (0x9E400) to one (0x70). I power up my board with PIO0_5 low and it hangs, it doesn't start. I connect in debugging with MultilinkUniversal (PEMicro) and verify that position 0x9E400 is set to 0x70. From what I understand from the LPC55S26 manual, during reset the CPU looks at pin PIO0_5 first of all, it would give the impression that if it is low it always enters ISP mode regardless of the bits in BOOT_CFG, but it is also strange that if so I don't find any sense in that PIO0_5 can be configured as UART reception.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 12:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1962695#M56915</guid>
      <dc:creator>alfredocyberhom</dc:creator>
      <dc:date>2024-09-26T12:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S26 PIO0_5 FC4_RXD use, ISP disable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1962944#M56917</link>
      <description>I prepared the program image for the Cyclone (from PEMicro), setting bits 4-6 of BOOT_CFG (0x9E400) to one (0x70). I power up my board with PIO0_5 low and it hangs, it doesn't start. I connect in debugging with MultilinkUniversal (PEMicro) and verify that position 0x9E400 is set to 0x70. From what I understand from the LPC55S26 manual, during reset the CPU looks at pin PIO0_5 first of all, it would give the impression that if it is low it always enters ISP mode regardless of the bits in BOOT_CFG, but it is also strange that if so I don't find any sense in that PIO0_5 can be configured as UART reception.</description>
      <pubDate>Thu, 26 Sep 2024 19:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1962944#M56917</guid>
      <dc:creator>alfredocyberhom</dc:creator>
      <dc:date>2024-09-26T19:58:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S26 PIO0_5 FC4_RXD use, ISP disable</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1963922#M56925</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167127"&gt;@alfredocyberhom&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;The problem arises because the boot mode selection (via PIO0_5 pin) takes precedence during reset, which causes the processor to jump to the ISP if the pin is low.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;To work around this issue, you can prevent the processor from entering the ISP mode by ensuring the state of PIO0_5 is high during reset. Since PIO0_5 is being used as a UART4 receiver (FC4_RXD), you have a couple of options:&lt;BR /&gt;You can add an external pull-up resistor (e.g., 10kΩ to 3.3V) to the PIO0_5 pin. This will ensure that PIO0_5 is high during reset, preventing the processor from entering ISP mode.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Hang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 29 Sep 2024 06:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S26-PIO0-5-FC4-RXD-use-ISP-disable/m-p/1963922#M56925</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-09-29T06:20:36Z</dc:date>
    </item>
  </channel>
</rss>