<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S36-EVK no contact via debugger after running TrustZone example in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-EVK-no-contact-via-debugger-after-running-TrustZone/m-p/1957520#M56883</link>
    <description>&lt;P&gt;I have tried out the TrustZone examples that comes with the LPC55S36 SDK from NXP's website using the IAR EWARM environment. I could debug this nicely and jump from secure start-up into the nonsecure part of the simple Hello World example.&lt;/P&gt;&lt;P&gt;Suddenly, however, I am locked out and can't debug anymore. Using BLHOST and starting the ISP-bootloader, I can run a ".... get-property 17" and see that the bootloader is now in SECURE mode. How did it jump in there?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I suppose this is irreversible?&lt;/P&gt;&lt;P&gt;And can I do anything to get back to debyugging?&lt;/P&gt;</description>
    <pubDate>Thu, 19 Sep 2024 09:14:45 GMT</pubDate>
    <dc:creator>jpholme</dc:creator>
    <dc:date>2024-09-19T09:14:45Z</dc:date>
    <item>
      <title>LPC55S36-EVK no contact via debugger after running TrustZone example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-EVK-no-contact-via-debugger-after-running-TrustZone/m-p/1957520#M56883</link>
      <description>&lt;P&gt;I have tried out the TrustZone examples that comes with the LPC55S36 SDK from NXP's website using the IAR EWARM environment. I could debug this nicely and jump from secure start-up into the nonsecure part of the simple Hello World example.&lt;/P&gt;&lt;P&gt;Suddenly, however, I am locked out and can't debug anymore. Using BLHOST and starting the ISP-bootloader, I can run a ".... get-property 17" and see that the bootloader is now in SECURE mode. How did it jump in there?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I suppose this is irreversible?&lt;/P&gt;&lt;P&gt;And can I do anything to get back to debyugging?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 09:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-EVK-no-contact-via-debugger-after-running-TrustZone/m-p/1957520#M56883</guid>
      <dc:creator>jpholme</dc:creator>
      <dc:date>2024-09-19T09:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S36-EVK no contact via debugger after running TrustZone example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-EVK-no-contact-via-debugger-after-running-TrustZone/m-p/1958130#M56891</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, could you let me know what was the example that you using? I will replay on my side.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 20 Sep 2024 00:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-EVK-no-contact-via-debugger-after-running-TrustZone/m-p/1958130#M56891</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-09-20T00:46:18Z</dc:date>
    </item>
  </channel>
</rss>