<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: CAN buffer issue.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1953394#M56844</link>
    <description>&lt;P&gt;Hi there,&lt;BR /&gt;&lt;BR /&gt;I'm using the LPC54628J512,&lt;BR /&gt;&lt;BR /&gt;I can try test on an example, however this code runs very deep and I don't think I will be able to reproduce the conditions needed to create the issue.&lt;BR /&gt;&lt;BR /&gt;I have had some success by using only buffer index [0] and using retries when it fails. For more context this issue is causing the timing of the CAN messages to become inconsistent as well as increasing the time between messages. Sometimes resulting in messages getting discarded.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 10:21:29 GMT</pubDate>
    <dc:creator>ArendZAR</dc:creator>
    <dc:date>2024-09-12T10:21:29Z</dc:date>
    <item>
      <title>CAN buffer issue.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1951063#M56828</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I have an issue with the fsl_mcan drivers that I'm not sure how to fix:&lt;BR /&gt;&lt;BR /&gt;In the function:&amp;nbsp;&lt;SPAN&gt;MCAN_TransferSendNonBlocking&lt;BR /&gt;&lt;BR /&gt;The code that checks if the tx buffer is IDLE (kMCAN_StateIdle == handle-&amp;gt;bufferState[xfer-&amp;gt;bufferIdx])&amp;nbsp; returns&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;kStatus_MCAN_TxBusy even though the line is completely IDLE&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;Eventually the Data will get sent but messages are lost here. Deleting this line of code as a test made the code work flawlessly, however, it is likely to cause errors in the future.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;How can I solve this problem? For extra information, I am sending the first type of message every 100ms, the second type of message every 150ms and a third type every 5 seconds or so.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 11:17:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1951063#M56828</guid>
      <dc:creator>ArendZAR</dc:creator>
      <dc:date>2024-09-10T11:17:51Z</dc:date>
    </item>
    <item>
      <title>Re: CAN buffer issue.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1953377#M56843</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234380"&gt;@ArendZAR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please tell me which chip? And does the issue can be reproduced on SDK demo?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 10:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1953377#M56843</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-09-12T10:06:30Z</dc:date>
    </item>
    <item>
      <title>Re: CAN buffer issue.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1953394#M56844</link>
      <description>&lt;P&gt;Hi there,&lt;BR /&gt;&lt;BR /&gt;I'm using the LPC54628J512,&lt;BR /&gt;&lt;BR /&gt;I can try test on an example, however this code runs very deep and I don't think I will be able to reproduce the conditions needed to create the issue.&lt;BR /&gt;&lt;BR /&gt;I have had some success by using only buffer index [0] and using retries when it fails. For more context this issue is causing the timing of the CAN messages to become inconsistent as well as increasing the time between messages. Sometimes resulting in messages getting discarded.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 10:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1953394#M56844</guid>
      <dc:creator>ArendZAR</dc:creator>
      <dc:date>2024-09-12T10:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: CAN buffer issue.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1960706#M56904</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234380"&gt;@ArendZAR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the situation you described, you can try adding a retry mechanism in the MCAN_TransferSendNonBlocking function. If the first check returns kStatus_MCAN_TxBusy, you can wait for a short period and then check again. For example:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;status_t MCAN_TransferSendNonBlocking(MCAN_Type *base, mcan_handle_t *handle, const mcan_transfer_t *xfer)&lt;BR /&gt;{&lt;BR /&gt;status_t result = kStatus_MCAN_TxBusy;&lt;BR /&gt;uint32_t retryCount = 0;&lt;/P&gt;
&lt;P&gt;while ((result == kStatus_MCAN_TxBusy) &amp;amp;&amp;amp; (retryCount &amp;lt; MAX_RETRIES))&lt;BR /&gt;{&lt;BR /&gt;if (kMCAN_StateIdle == handle-&amp;gt;bufferState[xfer-&amp;gt;bufferIdx])&lt;BR /&gt;{&lt;BR /&gt;// Buffer is idle, proceed with sending&lt;BR /&gt;result = kStatus_Success;&lt;BR /&gt;// Your existing send logic here&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;else&lt;BR /&gt;{&lt;BR /&gt;// Buffer is busy, wait and retry&lt;BR /&gt;SDK_DelayAtLeastUs(100, SDK_DEVICE_SYSCLK_CLOCKRATE); // Adjust delay as needed&lt;BR /&gt;retryCount++;&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;
&lt;P&gt;return result;&lt;BR /&gt;}&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 10:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-buffer-issue/m-p/1960706#M56904</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-09-24T10:27:32Z</dc:date>
    </item>
  </channel>
</rss>