<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPCXpresso824 MAX won't autobaud for ISP in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso824-MAX-won-t-autobaud-for-ISP/m-p/1951443#M56831</link>
    <description>&lt;P&gt;I have an&amp;nbsp;LPCXpresso824 MAX board. I know that it is working as I can run the SDK examples for the UART and of course "blinky".&lt;/P&gt;&lt;P&gt;I am trying to put it into ISP mode and load a file using &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Flash-Magic-Programing-LPC/ta-p/1152763" target="_self"&gt;Flashmagic&lt;/A&gt;. With blinky loaded (so I know if user code is running) I hold down SW2 and reset the board before releasing SW2.&lt;/P&gt;&lt;P&gt;This should put the board into ISP mode and I can see that my LED no longer blinks suggesting user code is not running.&lt;/P&gt;&lt;P&gt;I then try to synchronize using Flashmagic (9600 baud) but it times out as "failed to autobaud". I have tried:&lt;/P&gt;&lt;P&gt;1. Both settings for JP3 (board is RevC)&lt;/P&gt;&lt;P&gt;2. Restarting into ISP mode while holding SW2 both with "reset SW3" and by physically disconnecting/reconnecting the USB cable.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I must be missing something, what am I doing wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 10 Sep 2024 20:42:12 GMT</pubDate>
    <dc:creator>scruffmeister</dc:creator>
    <dc:date>2024-09-10T20:42:12Z</dc:date>
    <item>
      <title>LPCXpresso824 MAX won't autobaud for ISP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso824-MAX-won-t-autobaud-for-ISP/m-p/1951443#M56831</link>
      <description>&lt;P&gt;I have an&amp;nbsp;LPCXpresso824 MAX board. I know that it is working as I can run the SDK examples for the UART and of course "blinky".&lt;/P&gt;&lt;P&gt;I am trying to put it into ISP mode and load a file using &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Flash-Magic-Programing-LPC/ta-p/1152763" target="_self"&gt;Flashmagic&lt;/A&gt;. With blinky loaded (so I know if user code is running) I hold down SW2 and reset the board before releasing SW2.&lt;/P&gt;&lt;P&gt;This should put the board into ISP mode and I can see that my LED no longer blinks suggesting user code is not running.&lt;/P&gt;&lt;P&gt;I then try to synchronize using Flashmagic (9600 baud) but it times out as "failed to autobaud". I have tried:&lt;/P&gt;&lt;P&gt;1. Both settings for JP3 (board is RevC)&lt;/P&gt;&lt;P&gt;2. Restarting into ISP mode while holding SW2 both with "reset SW3" and by physically disconnecting/reconnecting the USB cable.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I must be missing something, what am I doing wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 20:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso824-MAX-won-t-autobaud-for-ISP/m-p/1951443#M56831</guid>
      <dc:creator>scruffmeister</dc:creator>
      <dc:date>2024-09-10T20:42:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824 MAX won't autobaud for ISP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso824-MAX-won-t-autobaud-for-ISP/m-p/1951833#M56832</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240210"&gt;@scruffmeister&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please make sure connect the correct UART pins. Use PIO0_0 as RXD and PIO0_4 as TXD.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1726040258438.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298491iEFAFCE0B4995B2F5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1726040258438.png" alt="Alice_Yang_0-1726040258438.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1726040258438.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Not the J3 on board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 07:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso824-MAX-won-t-autobaud-for-ISP/m-p/1951833#M56832</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-09-11T07:39:16Z</dc:date>
    </item>
  </channel>
</rss>