<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC54618J512 GPIO Pin Initial State Issue in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1950469#M56825</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls connect a 5K ohm pull-down resistor on the PIO4_16 pin. If you still see the high pulse during the start-up process, at this time, because the software has not begun to be executed, so software can not solve it. For hardware, the pull-down resistor is the only way I suppose.&lt;/P&gt;
&lt;P&gt;As I said it is a tough issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 10 Sep 2024 02:00:07 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-09-10T02:00:07Z</dc:date>
    <item>
      <title>LPC54618J512 GPIO Pin Initial State Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1947319#M56786</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have a custom PCB mounted with an LPC54618J512 controller. I have initially configured the GPIO pin (PIO4_16) as a digital output with an initial state set to low. This pin is used to switch an N-channel MOSFET.&lt;/P&gt;&lt;P&gt;During the booting period, the GPIO pin should remain low, but I am observing a 250 ms high pulse before it goes to the low state. I need the GPIO state to remain low throughout the booting period. This issue is not specific to any particular GPIO pin; it occurs across all GPIO pins. I am unsure why I am getting this 250 ms high pulse.&lt;/P&gt;&lt;P&gt;For reference, I am attaching the GPIO configuration screenshot. The yellow pulse represents the GPIO (PIO4_16) signals.&lt;/P&gt;&lt;P&gt;Any suggestions to resolve this issue would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 14:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1947319#M56786</guid>
      <dc:creator>nithin3200</dc:creator>
      <dc:date>2024-09-04T14:12:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618J512 GPIO Pin Initial State Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1947650#M56792</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the GPIO pin is in input mode in default after Reset, so the pin is subject to noise.&lt;/P&gt;
&lt;P&gt;Pls try to connect a pull-down resistor on the pin and check if the pulse appears or not after reset.&lt;/P&gt;
&lt;P&gt;If the pulse still appears after you connect a pull-down resistor, it is a tough issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 01:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1947650#M56792</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-09-05T01:47:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618J512 GPIO Pin Initial State Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1948715#M56807</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi@ xiangjun_rong&lt;/P&gt;&lt;P&gt;Thanks for the reply. We have already connected the pull-down resistor in the hardware. Are there any other issues we should check?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Nithin&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 04:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1948715#M56807</guid>
      <dc:creator>nithin3200</dc:creator>
      <dc:date>2024-09-06T04:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618J512 GPIO Pin Initial State Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1950469#M56825</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls connect a 5K ohm pull-down resistor on the PIO4_16 pin. If you still see the high pulse during the start-up process, at this time, because the software has not begun to be executed, so software can not solve it. For hardware, the pull-down resistor is the only way I suppose.&lt;/P&gt;
&lt;P&gt;As I said it is a tough issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 02:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1950469#M56825</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-09-10T02:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618J512 GPIO Pin Initial State Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1953013#M56839</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your prompt replay. As per your suggestion I connected the 5K ohm pull down resistor. The noise has been removed, and the issue is solved.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for your guidance.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Nithin&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 04:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618J512-GPIO-Pin-Initial-State-Issue/m-p/1953013#M56839</guid>
      <dc:creator>nithin3200</dc:creator>
      <dc:date>2024-09-12T04:37:09Z</dc:date>
    </item>
  </channel>
</rss>