<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProblems with the example KeyboardHost</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-the-example-KeyboardHost/m-p/523039#M5675</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by paulo on Thu Aug 30 12:56:24 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm testing the examples Example_KeyboardHost and Example_VirtualSerial on a plate LPCXPRESSO baseboard along with the link containing the micro LPC LPC 1769.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I run the project Example_KeyboardHost without connecting a USB cable to connector X3 containing a FT232RL connected to UART3 the program runs normally but when I connect the cable occurs the errors identified in the images below, it all before I connect the keyboard. If I run the program with the cable already connected it runs normally, but when I open a terminal application and point to that door he gives the same mistakes of the images below.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In case the project Example_VirtualSerial it works normally, but I just connect the USB cable to the connector X3 to encounter the same problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the case of the example he uses Example_KeyboardHost UART3 to send keystrokes via the keyboard, but as I said earlier, I just connect the cable to the problem below occurs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyone have any tips for me?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:43:21 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:43:21Z</dc:date>
    <item>
      <title>Problems with the example KeyboardHost</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-the-example-KeyboardHost/m-p/523039#M5675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by paulo on Thu Aug 30 12:56:24 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm testing the examples Example_KeyboardHost and Example_VirtualSerial on a plate LPCXPRESSO baseboard along with the link containing the micro LPC LPC 1769.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I run the project Example_KeyboardHost without connecting a USB cable to connector X3 containing a FT232RL connected to UART3 the program runs normally but when I connect the cable occurs the errors identified in the images below, it all before I connect the keyboard. If I run the program with the cable already connected it runs normally, but when I open a terminal application and point to that door he gives the same mistakes of the images below.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In case the project Example_VirtualSerial it works normally, but I just connect the USB cable to the connector X3 to encounter the same problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the case of the example he uses Example_KeyboardHost UART3 to send keystrokes via the keyboard, but as I said earlier, I just connect the cable to the problem below occurs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyone have any tips for me?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-the-example-KeyboardHost/m-p/523039#M5675</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:43:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with the example KeyboardHost</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-the-example-KeyboardHost/m-p/523040#M5676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpUSBlib team on Wed Sep 19 16:38:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Check the owners manual to make sure your jumpers are set correctly. That X3 connector doubles as a firmware upgrade port for Flashmagic and some of the signals are connected to reset based on the jumper settings by default.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-the-example-KeyboardHost/m-p/523040#M5676</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:43:22Z</dc:date>
    </item>
  </channel>
</rss>