<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1769 power question in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-power-question/m-p/523038#M5674</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CharlesM on Sat Feb 08 21:56:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using a LPC1769 based LPCxpresso board. The LPC Link board is attached and no jumper connections have been severed or altered from the default factory configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I apply +5V from a 7805 regulator to pin J6-2 (EXT_POWX) of the LPC1769 board, what should be done with pin J6-28 (VIO_3V3X)? Do I need an additional 3.3V regulator to power VIO_3V3X as well, or can that pin be left open?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;!--break--&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The schematics indicate it is an input when the board is externally powered via EXT_POWX (as opposed to self-powered through USB), but I'm not sure how the attached LPC-Link board affects the VIO_3V3/VIO_3V3X signals.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:57:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:57:58Z</dc:date>
    <item>
      <title>LPC1769 power question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-power-question/m-p/523038#M5674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CharlesM on Sat Feb 08 21:56:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using a LPC1769 based LPCxpresso board. The LPC Link board is attached and no jumper connections have been severed or altered from the default factory configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I apply +5V from a 7805 regulator to pin J6-2 (EXT_POWX) of the LPC1769 board, what should be done with pin J6-28 (VIO_3V3X)? Do I need an additional 3.3V regulator to power VIO_3V3X as well, or can that pin be left open?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;!--break--&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The schematics indicate it is an input when the board is externally powered via EXT_POWX (as opposed to self-powered through USB), but I'm not sure how the attached LPC-Link board affects the VIO_3V3/VIO_3V3X signals.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-power-question/m-p/523038#M5674</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:58Z</dc:date>
    </item>
  </channel>
</rss>