<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S36 ETM Trace with IAR</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-ETM-Trace-with-IAR/m-p/1942915#M56735</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, the LPC553x have ETM module and support trace function.&lt;/P&gt;
&lt;P&gt;But the trace function requires dedicated hardware device and software tools, pls refer to the an14330.pdf, which I attached. Although it focuses on the i.mxrt, it also adapts to LPC family.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Aug 2024 02:28:38 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-08-29T02:28:38Z</dc:date>
    <item>
      <title>LPC55S36 ETM Trace with IAR</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-ETM-Trace-with-IAR/m-p/1942314#M56732</link>
      <description>&lt;P&gt;How does one utilize ETM trace debugging on the LPC55S36?&lt;/P&gt;&lt;P&gt;I have activated the 5 pins P1_1, P0_24, P0_28, P0_29 and P0_30 with mode 5 and 6 resp. to activate the outputs.&lt;/P&gt;&lt;P&gt;I have experimented with Debugger, I-JET settings under Trace, but nothing really seems to activate the icon during debugging.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 13:36:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-ETM-Trace-with-IAR/m-p/1942314#M56732</guid>
      <dc:creator>jpholme</dc:creator>
      <dc:date>2024-08-28T13:36:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S36 ETM Trace with IAR</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-ETM-Trace-with-IAR/m-p/1942915#M56735</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, the LPC553x have ETM module and support trace function.&lt;/P&gt;
&lt;P&gt;But the trace function requires dedicated hardware device and software tools, pls refer to the an14330.pdf, which I attached. Although it focuses on the i.mxrt, it also adapts to LPC family.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 02:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S36-ETM-Trace-with-IAR/m-p/1942915#M56735</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-08-29T02:28:38Z</dc:date>
    </item>
  </channel>
</rss>