<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックVoltage level I/O pins</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Voltage-level-I-O-pins/m-p/1923191#M56574</link>
    <description>&lt;P&gt;LPC55S16. Some output pins have 0,2V-3,3V, while others&amp;nbsp;have 0,2V-2,0V. Why?&lt;/P&gt;&lt;P&gt;Have a look at my attachment.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
    <pubDate>Thu, 01 Aug 2024 16:17:21 GMT</pubDate>
    <dc:creator>FruitSalad1</dc:creator>
    <dc:date>2024-08-01T16:17:21Z</dc:date>
    <item>
      <title>Voltage level I/O pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Voltage-level-I-O-pins/m-p/1923191#M56574</link>
      <description>&lt;P&gt;LPC55S16. Some output pins have 0,2V-3,3V, while others&amp;nbsp;have 0,2V-2,0V. Why?&lt;/P&gt;&lt;P&gt;Have a look at my attachment.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 16:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Voltage-level-I-O-pins/m-p/1923191#M56574</guid>
      <dc:creator>FruitSalad1</dc:creator>
      <dc:date>2024-08-01T16:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage level I/O pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Voltage-level-I-O-pins/m-p/1925091#M56586</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238106"&gt;@FruitSalad1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The voltage range of output pins on an LPC55S16 microcontroller can vary depending on the specific pin and its configuration. Some pins are designed to work with a 3.3V logic level, while others are designed for a 2.0V logic level. This is due to the different internal circuitry and electrical characteristics of the pins.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Mon, 05 Aug 2024 08:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Voltage-level-I-O-pins/m-p/1925091#M56586</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-08-05T08:00:46Z</dc:date>
    </item>
  </channel>
</rss>