<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S28 Bricked after low power try! in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-Bricked-after-low-power-try/m-p/1923146#M56573</link>
    <description>&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;I don't have that board, but the LPC should have some kind of 'ISP' jumper or way to put it into bootloader mode. Have you tried that and load a 'blinky' or something similer from there?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Thu, 01 Aug 2024 15:43:06 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2024-08-01T15:43:06Z</dc:date>
    <item>
      <title>LPC55S28 Bricked after low power try!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-Bricked-after-low-power-try/m-p/1923018#M56572</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to develop with LPC55S28 into a custom board. Yesterday I wrote into a RTC register without initilialization and after that I can't reprogram the microcontroller anymore.&lt;/P&gt;&lt;P&gt;I don't know why... I read a lot of threads and article on the web like this:&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2022/03/10/recovering-bricked-lpc55sxx-evk-boards/" target="_self"&gt;https://mcuoneclipse.com/2022/03/10/recovering-bricked-lpc55sxx-evk-boards/&lt;/A&gt;&amp;nbsp; but nothing works...&lt;/P&gt;&lt;P&gt;The error message when I try to erase the microcontroller is:&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;Executing flash operation 'Erase' (Erase flash) - Thu Aug 01 14:46:50 CEST 2024
Checking MCU info...
Scanning for targets...
Executing flash action...
SEGGER J-Link Commander V7.84a (Compiled Dec 22 2022 16:13:07)
DLL version V7.84a, compiled Dec 22 2022 16:11:39
J-Link Command File read successfully.
Processing script file...
J-Link&amp;gt;ExitOnError 1
J-Link Commander will now exit on Error
J-Link&amp;gt;r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V12 compiled Jan 24 2024 12:06:13
Hardware version: V12.00
J-Link uptime (since boot): 0d 00h 21m 25s
S/N: 602004828
License(s): RDI, FlashBP, FlashDL, JFlash, GDB
USB speed mode: High speed (480 MBit/s)
VTref=3.606V
Target connection not established yet but required for command.
Device "LPC55S28" selected.
Connecting to target via SWD
ConfigTargetSettings() start
Disabling flash programming optimizations: Compare, SkipBlankDataOnProg
ConfigTargetSettings() end
InitTarget() start
InitTarget() end
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001)
Iterating through AP map to find AHB-AP to use
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
Failed to power up DAP
ConfigTargetSettings() start
Disabling flash programming optimizations: Compare, SkipBlankDataOnProg
ConfigTargetSettings() end
InitTarget() start
ERROR: Wrong DM-AP IDCODE detected: 0xFFFFFFFF
InitTarget() end
Cannot connect to target.
Script processing completed.
Unable to perform operation!
Command failed with exit code 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;What can I do to fix this issue?!&lt;/P&gt;&lt;P&gt;Best&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 12:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-Bricked-after-low-power-try/m-p/1923018#M56572</guid>
      <dc:creator>MarcoGiammarini</dc:creator>
      <dc:date>2024-08-01T12:58:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28 Bricked after low power try!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-Bricked-after-low-power-try/m-p/1923146#M56573</link>
      <description>&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;I don't have that board, but the LPC should have some kind of 'ISP' jumper or way to put it into bootloader mode. Have you tried that and load a 'blinky' or something similer from there?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 15:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-Bricked-after-low-power-try/m-p/1923146#M56573</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2024-08-01T15:43:06Z</dc:date>
    </item>
  </channel>
</rss>