<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC845-DAC in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917923#M56536</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;gusarambula,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have a work on the required DAC concept.Please Update ASAP.Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jul 2024 07:56:22 GMT</pubDate>
    <dc:creator>VIGNESH_BABU</dc:creator>
    <dc:date>2024-07-26T07:56:22Z</dc:date>
    <item>
      <title>LPC845-DAC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917067#M56527</link>
      <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Hi,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I'm using the LPCXpresso845-MAX board. I want to use the DAC1 mode via pin PIO0_29. With reference to the LPC845 user manual UM11029, I can observe that there is a DAC MODE bit (number 16) in the IOCON register for DAC0, PIO0_17, which needs to be set to utilize DAC0, but there is no matching bit for DAC1 in the IOCON register for PIO0_29.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;In PIO0_29, how do I adjust the DAC MODE for DAC1?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I saw your reply,&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;(There isn't this bit, no need config&amp;nbsp;DAC MODE bit.) but still this problem is not solved. Here I attached the configuration of DAC and SWM and IOCON register. So kindly update the solution for that problem.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 10:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917067#M56527</guid>
      <dc:creator>VIGNESH_BABU</dc:creator>
      <dc:date>2024-07-25T10:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845-DAC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917358#M56530</link>
      <description>&lt;P&gt;Hello Vignesh,&lt;/P&gt;
&lt;P&gt;You mention a reply, is this thread a continuation of a previous one? If so, would you please this thread as to allow better tracking of this issue?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 17:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917358#M56530</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2024-07-25T17:15:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845-DAC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917891#M56535</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have run your application code, it appears the DAC0 works fine, the PIO0_17 can output voltage of DAC0. But It appears that the DAC1 does not work, in detail, PIO0_29 can not output voltage of DAC1.&lt;/P&gt;
&lt;P&gt;I will report the issue to AE team and check something is missed in RM.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 07:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917891#M56535</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-07-26T07:19:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845-DAC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917923#M56536</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;gusarambula,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have a work on the required DAC concept.Please Update ASAP.Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 07:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1917923#M56536</guid>
      <dc:creator>VIGNESH_BABU</dc:creator>
      <dc:date>2024-07-26T07:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845-DAC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1919026#M56541</link>
      <description>&lt;P&gt;Please convey the reply ASAP .&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 04:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1919026#M56541</guid>
      <dc:creator>VIGNESH_BABU</dc:creator>
      <dc:date>2024-07-29T04:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845-DAC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1920078#M56553</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you use LPCXPresso845MAX board, this is the PIO0_29 pin connection. If you want to test the PIO0_29 pin voltage, you have to test the pin 2 of SJ15.&lt;/P&gt;
&lt;P&gt;I have tested your code, it is correct. when I output DAC 1023, the P0_29 pin voltage is 3.3V.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1722320375355.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290892i7235E3521EAA9A1E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1722320375355.png" alt="xiangjun_rong_0-1722320375355.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 06:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC/m-p/1920078#M56553</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-07-30T06:24:38Z</dc:date>
    </item>
  </channel>
</rss>