<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic verilog does not compile, how to setup mcuxpresso to compile verilog, lpc55s69 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/verilog-does-not-compile-how-to-setup-mcuxpresso-to-compile/m-p/1911642#M56489</link>
    <description>&lt;P&gt;i have a very simple verilog code to use plu(lpc55s69)&lt;/P&gt;&lt;P&gt;module test(a,b,c);&lt;BR /&gt;input a,b;&lt;BR /&gt;output c;&lt;BR /&gt;assign c=a^b;&lt;BR /&gt;endmodule&lt;/P&gt;&lt;P&gt;i click the "Apply verilog configuration"&amp;nbsp; it shows "provide source code fail to compile"&lt;/P&gt;&lt;P&gt;i have tried mcuxpresso ver 11.7,11.8.1, 11.10 etc all have same problem, i tried both verilog text and verilog file. all the same. is there anything need to configured in order to use this function?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Jul 2024 21:38:32 GMT</pubDate>
    <dc:creator>hhh</dc:creator>
    <dc:date>2024-07-18T21:38:32Z</dc:date>
    <item>
      <title>verilog does not compile, how to setup mcuxpresso to compile verilog, lpc55s69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/verilog-does-not-compile-how-to-setup-mcuxpresso-to-compile/m-p/1911642#M56489</link>
      <description>&lt;P&gt;i have a very simple verilog code to use plu(lpc55s69)&lt;/P&gt;&lt;P&gt;module test(a,b,c);&lt;BR /&gt;input a,b;&lt;BR /&gt;output c;&lt;BR /&gt;assign c=a^b;&lt;BR /&gt;endmodule&lt;/P&gt;&lt;P&gt;i click the "Apply verilog configuration"&amp;nbsp; it shows "provide source code fail to compile"&lt;/P&gt;&lt;P&gt;i have tried mcuxpresso ver 11.7,11.8.1, 11.10 etc all have same problem, i tried both verilog text and verilog file. all the same. is there anything need to configured in order to use this function?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 21:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/verilog-does-not-compile-how-to-setup-mcuxpresso-to-compile/m-p/1911642#M56489</guid>
      <dc:creator>hhh</dc:creator>
      <dc:date>2024-07-18T21:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: verilog does not compile, how to setup mcuxpresso to compile verilog, lpc55s69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/verilog-does-not-compile-how-to-setup-mcuxpresso-to-compile/m-p/1912000#M56494</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the PLU module is integrated in LPC5569, LPC804 and part of MCXN families, there is a dedicated PLU Config tools, which can generate code to initialize the PLU register based on your logic circuit.&lt;/P&gt;
&lt;P&gt;Pls refer to the doc.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_blank"&gt;https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It tells where to download PLU Config tools and the utilization of the tools.&lt;/P&gt;
&lt;P&gt;In detail, the PLU Config tools generate code which can initialize PLU registers, you can copy the code to MCUXPresso, compile, it is okay.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 07:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/verilog-does-not-compile-how-to-setup-mcuxpresso-to-compile/m-p/1912000#M56494</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-07-19T07:53:30Z</dc:date>
    </item>
  </channel>
</rss>