<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Flash operation error on LPC11U66JBD48</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-operation-error-on-LPC11U66JBD48/m-p/1909261#M56461</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222942"&gt;@Mr_Damian&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you go into ISP mode, then using Flash Magic erase all flash.&lt;/P&gt;
&lt;P&gt;It is possible to download an image into the flash on the target that will then prevent any further debug access or connections. The classic cases of this are:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The image contains code that sets the MCU clocks up "incorrectly".&lt;/LI&gt;
&lt;LI&gt;The image contains code that enables a watchdog timer.&lt;/LI&gt;
&lt;LI&gt;The image contains code that puts the MCU into a very low power mode.&lt;/LI&gt;
&lt;LI&gt;The image contains code that "switches off" some, or all of the multiplexed debug pins (JTAG/SWD).&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;About detail you can also refer to thread:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jul 2024 01:52:37 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2024-07-16T01:52:37Z</dc:date>
    <item>
      <title>Flash operation error on LPC11U66JBD48</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-operation-error-on-LPC11U66JBD48/m-p/1908472#M56455</link>
      <description>&lt;P&gt;Hi everyone,&lt;BR /&gt;&lt;BR /&gt;I'm using the above micro and I have a feeling that I have written to a memory that I should of not to and this is what I'm getting:&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mr_Damian_1-1721030217923.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288518i0A1FF48562B1F849/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Mr_Damian_1-1721030217923.png" alt="Mr_Damian_1-1721030217923.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was wondering if someone had a similar issue and managed to resolve it.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Best Damian&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 07:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-operation-error-on-LPC11U66JBD48/m-p/1908472#M56455</guid>
      <dc:creator>Mr_Damian</dc:creator>
      <dc:date>2024-07-15T07:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: Flash operation error on LPC11U66JBD48</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-operation-error-on-LPC11U66JBD48/m-p/1909261#M56461</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222942"&gt;@Mr_Damian&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you go into ISP mode, then using Flash Magic erase all flash.&lt;/P&gt;
&lt;P&gt;It is possible to download an image into the flash on the target that will then prevent any further debug access or connections. The classic cases of this are:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The image contains code that sets the MCU clocks up "incorrectly".&lt;/LI&gt;
&lt;LI&gt;The image contains code that enables a watchdog timer.&lt;/LI&gt;
&lt;LI&gt;The image contains code that puts the MCU into a very low power mode.&lt;/LI&gt;
&lt;LI&gt;The image contains code that "switches off" some, or all of the multiplexed debug pins (JTAG/SWD).&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;About detail you can also refer to thread:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 01:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-operation-error-on-LPC11U66JBD48/m-p/1909261#M56461</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-07-16T01:52:37Z</dc:date>
    </item>
  </channel>
</rss>