<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HOW READ AND WRIT LPC2129 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1902379#M56415</link>
    <description>Hello, I would like to know if, besides the J-Link, I need anything else to read the LPC2129. Maybe something like a base with resistors or something similar, in addition to the J-Link. Would that be necessary?</description>
    <pubDate>Mon, 08 Jul 2024 14:11:32 GMT</pubDate>
    <dc:creator>angelormonteiro</dc:creator>
    <dc:date>2024-07-08T14:11:32Z</dc:date>
    <item>
      <title>HOW READ AND WRIT LPC2129</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1896135#M56333</link>
      <description>&lt;P&gt;Hello!&amp;nbsp;&lt;BR /&gt;I´m Trying to Read (Connect) LPC2129 using a J-Link V9 and i just have this massages bellow:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="angelormonteiro_0-1719616133156.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/286282iA4A8F0239F1955B8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="angelormonteiro_0-1719616133156.png" alt="angelormonteiro_0-1719616133156.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;angelormonteiro_0-1719616133156.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Application log started&lt;BR /&gt;- J-Flash V7.96p (J-Flash compiled Jun 27 2024 16:02:07)&lt;BR /&gt;- JLinkARM.dll V7.96p (DLL compiled Jun 27 2024 16:01:41)&lt;BR /&gt;Reading flash device list [C:\Program Files\SEGGER\JLink_V796p\ETC/JFlash/Flash.csv] ...&lt;BR /&gt;- List of flash devices read successfully (451 Devices)&lt;BR /&gt;Reading MCU device list ...&lt;BR /&gt;- List of MCU devices read successfully (11229 Devices)&lt;BR /&gt;Opening project file [C:\Users\PainelJET\Desktop\EVNRUDE TESTE.jflash] ...&lt;BR /&gt;- Project opened successfully&lt;BR /&gt;No data file specified!&lt;BR /&gt;Failed to open data file [C:\Users\PainelJET\Desktop\]...&lt;BR /&gt;Probe/ Programmer firmware: J-Link V9 compiled May 7 2021 16:26:12&lt;BR /&gt;Probe/ Programmer S/N: 69667549&lt;BR /&gt;Reading entire flash chip ...&lt;BR /&gt;- Connecting ...&lt;BR /&gt;- ERROR: Failed to connect.&lt;BR /&gt;Could not perform custom init sequence.&lt;BR /&gt;- ERROR: Connect failed&lt;BR /&gt;- ERROR: Could not read target memory, not connected&lt;/P&gt;&lt;P&gt;Can some one help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 23:08:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1896135#M56333</guid>
      <dc:creator>angelormonteiro</dc:creator>
      <dc:date>2024-06-28T23:08:16Z</dc:date>
    </item>
    <item>
      <title>Re: HOW READ AND WRIT LPC2129</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1897940#M56362</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235669"&gt;@angelormonteiro&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can check the following issues.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;1. Check Connections:&lt;BR /&gt;• Ensure that all physical connections are secure.&lt;BR /&gt;• Double-check the wiring and pinout connections between the J-Link and the LPC2129.&lt;BR /&gt;2. Power Supply:&lt;BR /&gt;• Verify that the target board is properly powered.&lt;BR /&gt;• Measure the voltage to ensure it’s within the acceptable range for the LPC2129.&lt;BR /&gt;3. Correct Device Selection:&lt;BR /&gt;• Ensure that you have selected the correct device in the J-Flash project settings.&lt;BR /&gt;• Go to Project &amp;gt; Project Settings &amp;gt; CPU and confirm that the LPC2129 is selected.&lt;BR /&gt;4. Reset Pin:&lt;BR /&gt;• Ensure that the reset pin is correctly connected.&lt;BR /&gt;• Sometimes, manually holding the reset pin low while connecting can help.&lt;BR /&gt;5. Firmware Update:&lt;BR /&gt;• Make sure the firmware of your J-Link is up to date. You can update it using the J-Link Configurator tool.&lt;BR /&gt;6. Software Version:&lt;BR /&gt;• Ensure that you are using the latest version of J-Flash and JLinkARM.dll.&lt;BR /&gt;7. JTAG/SWD Mode:&lt;BR /&gt;• Verify that the correct mode (JTAG or SWD) is selected and matches the configuration of your target MCU.&lt;BR /&gt;8. Custom Init Sequence:&lt;BR /&gt;• If you have a custom init sequence, double-check it for any errors. You might want to temporarily disable it to see if the issue persists.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Hope this will help you.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;BR&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Hang&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 03:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1897940#M56362</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-07-03T03:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: HOW READ AND WRIT LPC2129</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1902379#M56415</link>
      <description>Hello, I would like to know if, besides the J-Link, I need anything else to read the LPC2129. Maybe something like a base with resistors or something similar, in addition to the J-Link. Would that be necessary?</description>
      <pubDate>Mon, 08 Jul 2024 14:11:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1902379#M56415</guid>
      <dc:creator>angelormonteiro</dc:creator>
      <dc:date>2024-07-08T14:11:32Z</dc:date>
    </item>
    <item>
      <title>Re: HOW READ AND WRIT LPC2129</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1905032#M56429</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235669"&gt;@angelormonteiro&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are only reading the LPC2129, you only need jlink and not anything else.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jul 2024 03:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HOW-READ-AND-WRIT-LPC2129/m-p/1905032#M56429</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-07-10T03:26:30Z</dc:date>
    </item>
  </channel>
</rss>