<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： Stuck in while (!(LPC_SYSCON-&amp;gt;SYSPLLCLKUEN &amp; 0x01));     /* Wait Until Updated       */ in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Stuck-in-while-LPC-SYSCON-gt-SYSPLLCLKUEN-0x01-Wait-Until/m-p/1894864#M56323</link>
    <description>&lt;P&gt;You may have used software simulator instead of a hardware emulator. If so, you can add an initialization file with the content "map 0x40000000,0x400FFFFF read write".&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jun 2024 05:25:38 GMT</pubDate>
    <dc:creator>tangtang78</dc:creator>
    <dc:date>2024-06-27T05:25:38Z</dc:date>
    <item>
      <title>Stuck in while (!(LPC_SYSCON-&gt;SYSPLLCLKUEN &amp; 0x01));     /* Wait Until Updated       */</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Stuck-in-while-LPC-SYSCON-gt-SYSPLLCLKUEN-0x01-Wait-Until/m-p/523355#M5991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Scribe on Tue Nov 27 11:38:14 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi guys,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been attempting to implement basic SPI flash in the mass sotrage example for 11Uxx in 0.98/a for a while, however find that whenever I include my flash file and call the setup function I get stuck in the following setup loop:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;while (!(LPC_SYSCON-&amp;gt;SYSPLLCLKUEN &amp;amp; 0x01));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait Until Updated&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What's making me lose my mind is that this loop should execute before any code as it's from system_LPC11UXX.c I don't have a clue how I got here. If I attempt to insert break-points it doesn't help, I get stuck here before I even reach the new code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the off chance this was a RAM space issue, I reduced a large memory structure in another file considerably to no avail, my new code doesn't use that much RAM so this seems unlikely...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm baffled guys, any idea?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:43:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Stuck-in-while-LPC-SYSCON-gt-SYSPLLCLKUEN-0x01-Wait-Until/m-p/523355#M5991</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:43:35Z</dc:date>
    </item>
    <item>
      <title>回复： Stuck in while (!(LPC_SYSCON-&gt;SYSPLLCLKUEN &amp; 0x01));     /* Wait Until Updated       */</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Stuck-in-while-LPC-SYSCON-gt-SYSPLLCLKUEN-0x01-Wait-Until/m-p/1894864#M56323</link>
      <description>&lt;P&gt;You may have used software simulator instead of a hardware emulator. If so, you can add an initialization file with the content "map 0x40000000,0x400FFFFF read write".&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 05:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Stuck-in-while-LPC-SYSCON-gt-SYSPLLCLKUEN-0x01-Wait-Until/m-p/1894864#M56323</guid>
      <dc:creator>tangtang78</dc:creator>
      <dc:date>2024-06-27T05:25:38Z</dc:date>
    </item>
  </channel>
</rss>