<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LCP55S16 USB0 and USB1 difference in hardware design in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1894509#M56316</link>
    <description>&lt;P&gt;Thanks, Alice for your response.&lt;/P&gt;&lt;P&gt;Given that there is no difference between USB0 and USB1 and USB1 can support FS, why the MCU has two separate USB PHYs?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the USB1 operates only in FS mode, can it be operated crystal-less as well?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jun 2024 14:42:43 GMT</pubDate>
    <dc:creator>JaehoonLee13</dc:creator>
    <dc:date>2024-06-26T14:42:43Z</dc:date>
    <item>
      <title>LCP55S16 USB0 and USB1 difference in hardware design</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1891656#M56284</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are designing a biomedical device which collects bio-data and streams out through USB using LCP55S16. There are two USB ports -USB0 for FS and USB1 for HS.&lt;/P&gt;&lt;P&gt;I understand that USB1 HS supports FS protocol. Presumably we are using only a full speed USB 2.0 then I guess either USB0 or USB1 work. However, I want to understand the difference between using USB0 and USB1 in hardware design perspective.&amp;nbsp;&lt;/P&gt;&lt;P&gt;After going through the datasheet, my understanding is USB0 can be operated crystal-less (no external 16MHz crystal needed) ,while USB1 requires the external crystal through xtal32N/xtal32P pins. Is this the only difference between USB0 and USB1? If so, I assume LCP55s16 MCU integrates two separate PHY for USB0 and USB1 (correct me if I am wrong).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JaehoonLee13_0-1718913250366.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285120iE91543FA93F3B211/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JaehoonLee13_0-1718913250366.png" alt="JaehoonLee13_0-1718913250366.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JaehoonLee13_0-1718913250366.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In summary, my questions are as follows:&lt;/P&gt;&lt;P&gt;1) Do only USB1 require an external crystal, while USB0 can operate crystal-lessly?&lt;/P&gt;&lt;P&gt;2) LCP55S16 has two separate USB PHY for USB0/USB1?&lt;/P&gt;&lt;P&gt;3) Is there any other difference between USB0 and USB1?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Jaehoon&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 19:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1891656#M56284</guid>
      <dc:creator>JaehoonLee13</dc:creator>
      <dc:date>2024-06-20T19:58:50Z</dc:date>
    </item>
    <item>
      <title>Re: LCP55S16 USB0 and USB1 difference in hardware design</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1894125#M56313</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235047"&gt;@JaehoonLee13&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1) Do only USB1 require an external crystal, while USB0 can operate crystal-lessly?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; USB0 full-speed device supporting crystal-less operation in device mode using the software library example in technical note&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/TN00065.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/TN00065.pdf&lt;/A&gt;&amp;nbsp;.&lt;/P&gt;
&lt;P&gt;2) LCP55S16 has two separate USB PHY for USB0/USB1?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; Yes.&lt;/P&gt;
&lt;P&gt;3) Is there any other difference between USB0 and USB1?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt;Almost no other difference.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 07:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1894125#M56313</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-06-26T07:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: LCP55S16 USB0 and USB1 difference in hardware design</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1894509#M56316</link>
      <description>&lt;P&gt;Thanks, Alice for your response.&lt;/P&gt;&lt;P&gt;Given that there is no difference between USB0 and USB1 and USB1 can support FS, why the MCU has two separate USB PHYs?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the USB1 operates only in FS mode, can it be operated crystal-less as well?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 14:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1894509#M56316</guid>
      <dc:creator>JaehoonLee13</dc:creator>
      <dc:date>2024-06-26T14:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: LCP55S16 USB0 and USB1 difference in hardware design</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1897437#M56354</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235047"&gt;@JaehoonLee13&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;"If the USB1 operates only in FS mode, can it be operated crystal-less as well? "&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-&amp;gt;&amp;gt; No, no matter HS mode or FS mode, USB1 must use external crystal.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 10:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S16-USB0-and-USB1-difference-in-hardware-design/m-p/1897437#M56354</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-07-02T10:53:28Z</dc:date>
    </item>
  </channel>
</rss>