<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Power up sequence of LPC55S1 when bypassing the internal DCDC in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1893776#M56309</link>
    <description>Thank you!</description>
    <pubDate>Tue, 25 Jun 2024 16:27:28 GMT</pubDate>
    <dc:creator>JaehoonLee13</dc:creator>
    <dc:date>2024-06-25T16:27:28Z</dc:date>
    <item>
      <title>Power up sequence of LPC55S1 when bypassing the internal DCDC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1888860#M56263</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are designing the implantable device using LPC55S1 MCU and want to bypass the internal DCDC converter to avoid using an inductor.&lt;/P&gt;&lt;P&gt;I have read this &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Properly-bypassing-LPC5500-s-internal-DCDC-converter/m-p/1888143/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExYRjhVUUwwNEZJSzRJfDE4ODgxNDN8U1VCU0NSSVBUSU9OU3xoSw" target="_self"&gt;post&lt;/A&gt;&amp;nbsp;on the forum and understood the requirement and the unused pin connection.&lt;/P&gt;&lt;P&gt;Still need to figure out what will be the proper power up sequence to supply the core voltage to MCU.&lt;/P&gt;&lt;P&gt;Both USB0 and USB1 are used&amp;nbsp; and the VBAT = 1.8V&amp;nbsp;&amp;nbsp;in our design, hence we do have 3 distinct voltage rails: 1.8V(VBAT), 3.3V(USB), 1.1V(Core)&lt;/P&gt;&lt;P&gt;Could you please guide the proper powering up sequence in such case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One additional question regarding using 1.2V for the core (I know it has already been discussed in the previous post) is that what would be the trade-off using 1.2V for all frequency range ( less than 100MHz), assuming that the supply is well controlled not to exceed the maximum rating of VDD_PMU (1.26Vmax_absolute)?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JaehoonLee13_0-1718645059103.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284495iE073FD14B807CEDD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JaehoonLee13_0-1718645059103.png" alt="JaehoonLee13_0-1718645059103.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JaehoonLee13_0-1718645059103.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Jaehoon&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 17:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1888860#M56263</guid>
      <dc:creator>JaehoonLee13</dc:creator>
      <dc:date>2024-06-17T17:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: Power up sequence of LPC55S1 when bypassing the internal DCDC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1889215#M56264</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you have power supply rails:&lt;/P&gt;
&lt;P&gt;1.8V for for VDD, VDDA,Vrefp, VBAT_DCDC, VBAT_PMU pins&lt;/P&gt;
&lt;P&gt;3.3V for&amp;nbsp; USB0_3V3, USB1_3V3 pins&lt;/P&gt;
&lt;P&gt;1.1V for VDD_PMU&lt;/P&gt;
&lt;P&gt;The 1.8V&amp;nbsp; starts-up firstly, the 1.1V appears secondly. The USBx_3v3 pins provide power for only USB module, they can appear anytime.&lt;/P&gt;
&lt;P&gt;Anyway, we suggest you use internal DC/Dc converter.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 07:59:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1889215#M56264</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-06-18T07:59:32Z</dc:date>
    </item>
    <item>
      <title>Re: Power up sequence of LPC55S1 when bypassing the internal DCDC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1889682#M56267</link>
      <description>&lt;P&gt;Thanks XiangJun for your reply.&lt;/P&gt;&lt;P&gt;Could you please explain more details of the potential risks of not using an internal DCDC?&lt;/P&gt;&lt;P&gt;Is it purely because of setting a different voltage level depending on the operating frequency? What is the downside of using a higher voltage (such as 1.2V) for all frequency range? Maybe more power consumption?&lt;/P&gt;&lt;P&gt;I would like to understand the trade-offs between using an internal DCDC versus external LDO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Jaehoon&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 16:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1889682#M56267</guid>
      <dc:creator>JaehoonLee13</dc:creator>
      <dc:date>2024-06-18T16:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: Power up sequence of LPC55S1 when bypassing the internal DCDC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1889887#M56270</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LDO can provide stable output supply voltage with low efficiency, while the DC/DC converter can provide output supply voltage with ripple but high efficiency.&lt;/P&gt;
&lt;P&gt;Regarding the recommendation of internal DC/Dc converter, based on AE team advise, we never fully tested for using external LDO for the VDD_PMU power supply.&lt;/P&gt;
&lt;P&gt;But I think it is okay, you can use 1.2V LDO for the VDD_PMU, which will cover all the core clock frequency.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 01:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1889887#M56270</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-06-19T01:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: Power up sequence of LPC55S1 when bypassing the internal DCDC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1893776#M56309</link>
      <description>Thank you!</description>
      <pubDate>Tue, 25 Jun 2024 16:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1893776#M56309</guid>
      <dc:creator>JaehoonLee13</dc:creator>
      <dc:date>2024-06-25T16:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: Power up sequence of LPC55S1 when bypassing the internal DCDC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1900757#M56401</link>
      <description>&lt;P&gt;I am facing the same issue yestoday, now I found this. Thanks.&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jul 2024 07:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-up-sequence-of-LPC55S1-when-bypassing-the-internal-DCDC/m-p/1900757#M56401</guid>
      <dc:creator>shreiyib</dc:creator>
      <dc:date>2024-07-06T07:59:40Z</dc:date>
    </item>
  </channel>
</rss>