<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC11U35FHI33/501 USB HID ROM API NAK Issue in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U35FHI33-501-USB-HID-ROM-API-NAK-Issue/m-p/1893309#M56304</link>
    <description>&lt;P&gt;I am working on LPC11U35FHI33/501 as USB HID device using ROM API(USB on-chip driver).&lt;/P&gt;&lt;P&gt;&amp;lt; Issue &amp;gt;&lt;BR /&gt;HID Device send NAK to USB host when USB host send OUT transaction (Interrupt out) to device.&lt;BR /&gt;At first, ACK is returned normally, but at a certain point it becomes NAK, and after that NAK is returned always.&lt;/P&gt;&lt;P&gt;&amp;lt; Question &amp;gt;&lt;BR /&gt;What are the conditions under which a device returns a NAK?&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jun 2024 04:43:47 GMT</pubDate>
    <dc:creator>BBQ</dc:creator>
    <dc:date>2024-06-25T04:43:47Z</dc:date>
    <item>
      <title>LPC11U35FHI33/501 USB HID ROM API NAK Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U35FHI33-501-USB-HID-ROM-API-NAK-Issue/m-p/1893309#M56304</link>
      <description>&lt;P&gt;I am working on LPC11U35FHI33/501 as USB HID device using ROM API(USB on-chip driver).&lt;/P&gt;&lt;P&gt;&amp;lt; Issue &amp;gt;&lt;BR /&gt;HID Device send NAK to USB host when USB host send OUT transaction (Interrupt out) to device.&lt;BR /&gt;At first, ACK is returned normally, but at a certain point it becomes NAK, and after that NAK is returned always.&lt;/P&gt;&lt;P&gt;&amp;lt; Question &amp;gt;&lt;BR /&gt;What are the conditions under which a device returns a NAK?&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 04:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U35FHI33-501-USB-HID-ROM-API-NAK-Issue/m-p/1893309#M56304</guid>
      <dc:creator>BBQ</dc:creator>
      <dc:date>2024-06-25T04:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11U35FHI33/501 USB HID ROM API NAK Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U35FHI33-501-USB-HID-ROM-API-NAK-Issue/m-p/1897293#M56346</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235453"&gt;@BBQ&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Recommend you check the application code in USB device. This is depends on device application code.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 08:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U35FHI33-501-USB-HID-ROM-API-NAK-Issue/m-p/1897293#M56346</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-07-02T08:05:31Z</dc:date>
    </item>
  </channel>
</rss>