<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S16 - CANOpen Autostart?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892651#M56296</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196991"&gt;@JK_265&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes,&amp;nbsp;according to this Note message, this is a &lt;SPAN&gt;precompiled CANOpen library.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hope this will help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 24 Jun 2024 07:05:57 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-06-24T07:05:57Z</dc:date>
    <item>
      <title>LPC55S16 - CANOpen Autostart?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892186#M56291</link>
      <description>&lt;P&gt;Using LPC55S16 with CANOpen stack from ESA as provided by MCUXpresso.&lt;BR /&gt;Per the documentation, if I modify the file nodecfg.h so that AUTOSTART is defined as 1 instead of 0, then my node should automatically enter the CANOpen operational state.&amp;nbsp; I have tried this, but after reset the node is still pre-operational.&amp;nbsp; Can anyone help?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jun 2024 14:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892186#M56291</guid>
      <dc:creator>JK_265</dc:creator>
      <dc:date>2024-06-21T14:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 - CANOpen Autostart?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892205#M56292</link>
      <description>&lt;P&gt;I just noticed these comments at the top of the nodecfg file:&lt;BR /&gt;&lt;BR /&gt;/*&lt;BR /&gt;* Note: All settings below are for informational purposes only and&lt;BR /&gt;* must not be changed in projects that use the NXP SDK library&lt;BR /&gt;* version of MicroCANopen. Changes here will not affect the&lt;BR /&gt;* delivered library and may lead to applications that fail to&lt;BR /&gt;* build or perform.&lt;BR /&gt;*/&lt;BR /&gt;&lt;BR /&gt;So, does that mean I am out of luck, because NXP delivers the precompiled CANOpen library and I can't rebuild it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jun 2024 14:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892205#M56292</guid>
      <dc:creator>JK_265</dc:creator>
      <dc:date>2024-06-21T14:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 - CANOpen Autostart?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892651#M56296</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196991"&gt;@JK_265&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes,&amp;nbsp;according to this Note message, this is a &lt;SPAN&gt;precompiled CANOpen library.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hope this will help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 07:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-CANOpen-Autostart/m-p/1892651#M56296</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-24T07:05:57Z</dc:date>
    </item>
  </channel>
</rss>