<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 MCUXpresso | Build Artifact | Executable type changes</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-Build-Artifact-Executable-type-changes/m-p/1889991#M56271</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Currently, I am working on LPC1788 Open library package. I can't able to generate a hex file because of the static library option. I need to change the build artifact type from static library to executable method. Is there any possible?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Jun 2024 04:24:18 GMT</pubDate>
    <dc:creator>Balaji_KG</dc:creator>
    <dc:date>2024-06-19T04:24:18Z</dc:date>
    <item>
      <title>MCUXpresso | Build Artifact | Executable type changes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-Build-Artifact-Executable-type-changes/m-p/1889991#M56271</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Currently, I am working on LPC1788 Open library package. I can't able to generate a hex file because of the static library option. I need to change the build artifact type from static library to executable method. Is there any possible?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 04:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-Build-Artifact-Executable-type-changes/m-p/1889991#M56271</guid>
      <dc:creator>Balaji_KG</dc:creator>
      <dc:date>2024-06-19T04:24:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso | Build Artifact | Executable type changes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-Build-Artifact-Executable-type-changes/m-p/1890315#M56275</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215923"&gt;@Balaji_KG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, it is possible to change the build artifact type from static library to executable. You can do this by modifying the project settings in MCUXpresso.&lt;/P&gt;
&lt;P&gt;Here are the steps:&lt;/P&gt;
&lt;P&gt;1. Open your project in MCUXpresso.&lt;BR /&gt;2. Go to Project -&amp;gt; Properties.&lt;BR /&gt;3. In the Properties window, go to C/C++ Build -&amp;gt; Settings.&lt;BR /&gt;4. In the Settings tab, you will see a field called "Build Artifact".&lt;BR /&gt;5. Change the "Build Artifact" from "Static Library" to "Executable".&lt;BR /&gt;6. Click on "Apply" and then "OK" to save the changes.&lt;BR /&gt;7. Now, try to build your project again. It should generate a hex file instead of a static library.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 10:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-Build-Artifact-Executable-type-changes/m-p/1890315#M56275</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-19T10:40:46Z</dc:date>
    </item>
  </channel>
</rss>