<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックWant to add UART communication in NFCrdlibEx4_Mifareclassic code</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-add-UART-communication-in-NFCrdlibEx4-Mifareclassic-code/m-p/1888196#M56255</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using CLEV6630B board for RFID reader and want to read/write on Mifare classic card.&lt;/P&gt;&lt;P&gt;I am using NFCrdlibEx4_Mifareclassic library code. I want to add UART communication in this code so that I can connect the board to PC over serial and send the card information to PC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to develop PC based software through which I can send the commands to the CLEV6630B board to write some data in the Mifare Classic card, read data from Mifare Classic card etc. In short I want to add UART interface on TXD0 and RXD0 (which is available on&amp;nbsp;CLEV6630B) in&amp;nbsp;NFCrdlibEx4_Mifareclassic code&lt;/P&gt;&lt;P&gt;Please guide. Please share some sample code.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Sat, 15 Jun 2024 11:31:35 GMT</pubDate>
    <dc:creator>suhas_badve1</dc:creator>
    <dc:date>2024-06-15T11:31:35Z</dc:date>
    <item>
      <title>Want to add UART communication in NFCrdlibEx4_Mifareclassic code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-add-UART-communication-in-NFCrdlibEx4-Mifareclassic-code/m-p/1888196#M56255</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using CLEV6630B board for RFID reader and want to read/write on Mifare classic card.&lt;/P&gt;&lt;P&gt;I am using NFCrdlibEx4_Mifareclassic library code. I want to add UART communication in this code so that I can connect the board to PC over serial and send the card information to PC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to develop PC based software through which I can send the commands to the CLEV6630B board to write some data in the Mifare Classic card, read data from Mifare Classic card etc. In short I want to add UART interface on TXD0 and RXD0 (which is available on&amp;nbsp;CLEV6630B) in&amp;nbsp;NFCrdlibEx4_Mifareclassic code&lt;/P&gt;&lt;P&gt;Please guide. Please share some sample code.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Sat, 15 Jun 2024 11:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-add-UART-communication-in-NFCrdlibEx4-Mifareclassic-code/m-p/1888196#M56255</guid>
      <dc:creator>suhas_badve1</dc:creator>
      <dc:date>2024-06-15T11:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: Want to add UART communication in NFCrdlibEx4_Mifareclassic code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-add-UART-communication-in-NFCrdlibEx4-Mifareclassic-code/m-p/1889771#M56268</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187871"&gt;@suhas_badve1&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;We will continue the communication in your internal ticket.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 20:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-add-UART-communication-in-NFCrdlibEx4-Mifareclassic-code/m-p/1889771#M56268</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-06-18T20:23:44Z</dc:date>
    </item>
  </channel>
</rss>