<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Regards LPC1788 FlexWire Interface Support</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regards-LPC1788-FlexWire-Interface-Support/m-p/1877828#M56170</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212844"&gt;@gowtham_pmt1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, the LPC1788 can support FlexWire Interface through UART. The TPS929240-Q1 LED driver is designed to be controlled by a microcontroller via the FlexWire interface, which uses a serial communication protocol similar to SPI.&lt;/P&gt;
&lt;P&gt;To control the TPS929240-Q1 LED driver with the LPC1788, you will need to use one of the LPC1788's UART ports and configure it to communicate with the FlexWire interface on the TPS929240-Q1. This involves setting up the appropriate baud rate, data bits, parity, and stop bits for the UART communication, as well as implementing the necessary software protocol to send and receive data over the FlexWire interface.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
    <pubDate>Thu, 30 May 2024 03:45:37 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-05-30T03:45:37Z</dc:date>
    <item>
      <title>Regards LPC1788 FlexWire Interface Support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regards-LPC1788-FlexWire-Interface-Support/m-p/1877309#M56166</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to control&amp;nbsp;TPS929240-Q1 Led driver by LPC1788.&lt;/P&gt;&lt;P&gt;Is LPC1788 can support FlexWire Interface through UART or any other way?&lt;/P&gt;&lt;P&gt;Kindly solve my doubt.&lt;/P&gt;</description>
      <pubDate>Wed, 29 May 2024 13:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Regards-LPC1788-FlexWire-Interface-Support/m-p/1877309#M56166</guid>
      <dc:creator>gowtham_pmt1</dc:creator>
      <dc:date>2024-05-29T13:00:36Z</dc:date>
    </item>
    <item>
      <title>Re: Regards LPC1788 FlexWire Interface Support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regards-LPC1788-FlexWire-Interface-Support/m-p/1877828#M56170</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212844"&gt;@gowtham_pmt1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, the LPC1788 can support FlexWire Interface through UART. The TPS929240-Q1 LED driver is designed to be controlled by a microcontroller via the FlexWire interface, which uses a serial communication protocol similar to SPI.&lt;/P&gt;
&lt;P&gt;To control the TPS929240-Q1 LED driver with the LPC1788, you will need to use one of the LPC1788's UART ports and configure it to communicate with the FlexWire interface on the TPS929240-Q1. This involves setting up the appropriate baud rate, data bits, parity, and stop bits for the UART communication, as well as implementing the necessary software protocol to send and receive data over the FlexWire interface.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Thu, 30 May 2024 03:45:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Regards-LPC1788-FlexWire-Interface-Support/m-p/1877828#M56170</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-05-30T03:45:37Z</dc:date>
    </item>
  </channel>
</rss>