<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Regarding the timer external clock operation of the LPC800 series</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-the-timer-external-clock-operation-of-the-LPC800/m-p/1875112#M56151</link>
    <description>&lt;P&gt;Set the internal clock to 4MHz and operate it,&lt;BR /&gt;Is it possible to use an external clock (40kHz) only for the timer operation?&lt;/P&gt;&lt;P&gt;Uses an external clock only for the timer operation clock.&lt;BR /&gt;I would like to operate other functions using the internal clock.&lt;/P&gt;</description>
    <pubDate>Mon, 27 May 2024 02:45:30 GMT</pubDate>
    <dc:creator>Ryo10</dc:creator>
    <dc:date>2024-05-27T02:45:30Z</dc:date>
    <item>
      <title>Regarding the timer external clock operation of the LPC800 series</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-the-timer-external-clock-operation-of-the-LPC800/m-p/1875112#M56151</link>
      <description>&lt;P&gt;Set the internal clock to 4MHz and operate it,&lt;BR /&gt;Is it possible to use an external clock (40kHz) only for the timer operation?&lt;/P&gt;&lt;P&gt;Uses an external clock only for the timer operation clock.&lt;BR /&gt;I would like to operate other functions using the internal clock.&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 02:45:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-the-timer-external-clock-operation-of-the-LPC800/m-p/1875112#M56151</guid>
      <dc:creator>Ryo10</dc:creator>
      <dc:date>2024-05-27T02:45:30Z</dc:date>
    </item>
  </channel>
</rss>