<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S16 MCAN PSR Functions question</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1869255#M56104</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As the name of PSR implies, the ACT bits reflect the state of CAN bus, if you want to see if the ACT bits change or not based on CAN bus action, you can have a test.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;You can modify the code like the attached code. I use the example for LPC5506 instead of LPC5516.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Hope it can help you&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;BR&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;XiangJun Rong&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 21 May 2024 02:26:12 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-05-21T02:26:12Z</dc:date>
    <item>
      <title>LPC55S16 MCAN PSR Functions question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1869101#M56100</link>
      <description>&lt;P&gt;for my project I'm trying to utilize the register to better control the mcan module how i need and i see this PSR ACT portion give me part of what I'm looking to do, but it doesn't seem to work as stated in the Manuel. when testing I'm not seeing ACT change and always indicates idle. how is the ACT portion of the PSR suppose to work?&lt;/P&gt;</description>
      <pubDate>Mon, 20 May 2024 19:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1869101#M56100</guid>
      <dc:creator>jmorel</dc:creator>
      <dc:date>2024-05-20T19:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 MCAN PSR Functions question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1869255#M56104</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As the name of PSR implies, the ACT bits reflect the state of CAN bus, if you want to see if the ACT bits change or not based on CAN bus action, you can have a test.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;You can modify the code like the attached code. I use the example for LPC5506 instead of LPC5516.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Hope it can help you&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;BR&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;XiangJun Rong&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 May 2024 02:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1869255#M56104</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-05-21T02:26:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 MCAN PSR Functions question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1877568#M56167</link>
      <description>&lt;P&gt;in the end still didn't see any actions from the ACT portion ended up just following the IR and IE register as a status of the module.&lt;/P&gt;</description>
      <pubDate>Wed, 29 May 2024 20:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-MCAN-PSR-Functions-question/m-p/1877568#M56167</guid>
      <dc:creator>jmorel</dc:creator>
      <dc:date>2024-05-29T20:00:57Z</dc:date>
    </item>
  </channel>
</rss>