<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックGPDMA Request Line for Uart1 and Uart4</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Request-Line-for-Uart1-and-Uart4/m-p/522972#M5608</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mohitm on Sat Jan 18 05:29:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC1778 for a robotic application. I wish to use uart 1 and uart 4 for communicating with external devices. I have dma based transmission enabled on both uart. But since they share the same dma request line (line 12 ) the transmission of both uart is getting corrupted when they are used simultaneously. Same problem is not observed when using uart0 and uart1. Is this the expected behavior ? Apart from using different uart instead of uart4 which will require us to make a new hardware is there a possible solution for this.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:00:15 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:00:15Z</dc:date>
    <item>
      <title>GPDMA Request Line for Uart1 and Uart4</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Request-Line-for-Uart1-and-Uart4/m-p/522972#M5608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mohitm on Sat Jan 18 05:29:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC1778 for a robotic application. I wish to use uart 1 and uart 4 for communicating with external devices. I have dma based transmission enabled on both uart. But since they share the same dma request line (line 12 ) the transmission of both uart is getting corrupted when they are used simultaneously. Same problem is not observed when using uart0 and uart1. Is this the expected behavior ? Apart from using different uart instead of uart4 which will require us to make a new hardware is there a possible solution for this.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Request-Line-for-Uart1-and-Uart4/m-p/522972#M5608</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:00:15Z</dc:date>
    </item>
  </channel>
</rss>