<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: A C Example for measuring sub 2pF capacitance change using a LPC804 chip</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863993#M56017</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;At the time being, SDK is developed by NXP dedicated software team, there is not any channel for external user code to be embedded in SDK package.&lt;/P&gt;
&lt;P&gt;If you have recommendation to add code for a general application field, you can submit request, I can submit it to SDK team.&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 13 May 2024 03:42:55 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-05-13T03:42:55Z</dc:date>
    <item>
      <title>A C Example for measuring sub 2pF capacitance change using a LPC804 chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863701#M56010</link>
      <description>&lt;P&gt;Here is an &lt;STRONG&gt;Example of measuring sub 2pF Capacitance change using a LPC804&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;A few questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What is process to get an example like this added to the examples in the SDK?&lt;/LI&gt;&lt;LI&gt;What is best way to learn to port this to use the PLU instead of explicit C Code?&lt;/LI&gt;&lt;LI&gt;What is the best process for sharing content like this with other LPC users?&lt;/LI&gt;&lt;LI&gt;Is it worth porting to use Analog comparator rather than gate logic transition threshold? What benefit will we likely gain?&lt;/LI&gt;&lt;LI&gt;Does anybody see a way to increase true resolution by a factor of 10 with clever circuit changes. This would allow either less jitter or less oversampling both of which could save power.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/*
 * Copyright 2024 RainAmp.Com
 * All rights reserved.
 *
 * License MIT but please pay for enhancements.
 * or custom engineering  info@RainAmp.com
 */

/**
 * @file    LPC804_read_variable_capacitor_logic_level_transition
 *
 * @brief   Measures Variable Capacitance such as water level changing
 *          between two electrodes by measuring changes in time required for
 *          charge to drop from charge level to gate transition voltage.
 *          This version works on any CPU with sufficient speed even if
 *          they do not have analog comparator or an accurate timer.
 *
 *          CIRCUIT Information:
 *            IO21 = SENSE PIN  (NET SENSE)
 *              Configure as Input with pullup inactive
 *            IO28 = Drive PIN  (NET DRIVE)
 *              Configure as output with default low
 *            IO25 = LED PIN
 *              Configure as output with default low
 *
 *            LED PIN -&amp;gt; 4.7K resistor -&amp;gt; GND
 *            NET-DRIVE -&amp;gt; 28M resistor (R1) -&amp;gt; NET-SENSE
 *            NET-DRIVE -&amp;gt; Diode (D1) -&amp;gt; NET-SENSE
 *            NET-SENSE -&amp;gt; 100pf CAP (C1) -&amp;gt; GND
 *            NET-SENSE -&amp;gt; Variable Cap Positive Electrode
 *            GND -&amp;gt; Variable CAP Negative Electrode
 *            Output on standard Pins at 9600 baud.
 *
 *            NOTES:
 *              Diode D1 current flow from Net-Drive to Net-&amp;gt;Sense to allow fast
 *              charging of sense pin.
 *
 *              Discharge of variable capacitor + CAP(c1) circuit is through
 *              resistor R1 into IO25 (DRIVE)
 *
 *              Capacitor C1 is required to be this large on LPC chip to
 *              overcome some leakage on the pin it self. Other chips may
 *              require a larger or smaller level.
 *
 *              This is optimized to sense relatively small capacitance changes
 *              where a 1% change in fluid level may only yield a sub 1pf change
 *              in capacitance. When using larger capacitors will need to reduce
 *              size of 28M resistor. For very large capacitors will need to use
 *              Drive pin to activate a external switch to drive charge cycle or
 *              it could draw excess current from IO28. When using larger variable
 *              capacitors then add a 4.8K resistor between DRIVE and Diode to
 *              limit current drawn from pin to safe level.
 *
 *              This CPU is at the lower end of speed necessary to sense capacitance
 *              changes this small using this technique.  A better
 *              approach is to use VSS such as 12V with an Analog comparator where
 *              we drive two output pins from analog comparator PHigh is high when
 *              SenseCircuit is above VSS * 0.9  and PLOW is high when SenseCircuit
 *              is below VSS * 0.1.  Then use a switch driven by NET-DRIVE to
 *              charge the circuit and discharge to ground through a High Resistance
 *              bleed resistor.   Then we cycle the pins between high and low as
 *              fast as we can with reasonable de-bounce and measure how many cycles
 *              can be accomplished in a defined time such as 1ms. It requires adding
 *              an analog comparator or opAmp with two circuits but the larger switch
 *              of VSS provides longer transition times that slower CPU can better deal
 *              with. This version requires accurate  time keeping.
 *
 *              Next step convert this to use the LPC804 on-board analog comparator
 *              rather than logic level transitions. Also see if we can duplicate
 *              the logic using the PLU rather than explicit looping in C.
 *
 *           ---------
 *           Readings
 *           ---------
 *            Please note after taking these readings I changed
 *            the algorithm to increase scale by 100 which allowed
 *            access to finer resolution of data at expense of greater
 *            jitter.  Please multiply all these numbers by 100 until
 *            until we update the measurements.
 *
 *            No 100 pf capacitor in circuit - 1
 *
 *            With 100pf capacitor in circuit - 27
 *
 *            Water bottle with + and - electrodes on
 *              electrodes on outside opposite side
 *              of 1 liter bottle. bottle
                Change from 0% to 70% = 103 - 35 = 68
                Average change per % of fluid change = 0.9814
                  count units

                due to changing shape of bottle and electrode
                the most accurate  approximation would be from
                10% full to 70% full.  103 - 49 = 54.
                54 units / 60% change = 0.9 count units per 1% water
                level change. Could use approximation between points to
                get more accurate estimation with variable shaped
                tanks.

 *              Empty bottle - 35
 *              Bottle with 10ml fluid - 38
 *              Bottle with 20ml fluid - 41
 *              Bottle with 100ml fluid - 49
 *              Bottle with 200ml Fluid - 58
 *              Bottle with 300ml Fluid - 68
 *              Bottle with 400ml fluid - 76
 *              Bottle with 500ml fluid - 86
 *              Bottle with 600ml fluid - 93
 *              Bottle with 700ml fluid - 103*
 *              Bottle 100% full - 127
 *              Human touch positive electrode full bottle - 775
 *              Human touch both electrodes full bottle - 1378
 *              Human touch positive electrode empty bottle - 532
 *              Human touch both positive and neg electrodes empty bottle - 1454
 *              0.047 uF capacitor instead of water bottle of - 24776
 *                 capacitor was 5% rated but 10 years old ceramic.
 *                 A change of 24776 -27 =  change of 24749 or
 *                 a change of 526574.46 per uf or 0.00000189906 uf per
 *                 count unit.  This converts to 1.89906 pF per count
 *                 unit.  A 5% variation in capacitor would yield
 *                 a range of 1.804 to 1.994013 pF per count unit.
 *
 *              0.01 uF capacitor instead of water bottle - 5664
 *                Capacitor was 5% rate but 10 year old ceramic
 *                a change of 5664 - 27 = 5637 or 563700 count units per
 *                uF or 0.00017739932 uF per count unit or 1.774 pF
 *                per count unit.   A 5% variation in capacitor
 *                would put this in the range of 1.6853pf to 1.8627 pF
 *                per count unit.
 *
 *              Using an average of our two reference capacitors
 *              yields  1.83 pF per count unit and we know our average
 *              per 1% change in water was 0.9 so we can determine
 *              that a 1% change in water level yields a 1.653pF
 *              change in capacitance.
 *
 *              Please Note these tests were ran with Debug mode
 *              compilation and ran without the debugger running.
 *
 *
 *          Application entry point.
 */
#include &amp;lt;stdio.h&amp;gt;
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "LPC804.h"
#include "fsl_debug_console.h"
//#undef PRINTDELAY
#define PRINTDELAY

#define posCntDeBounce 125
#define  negCntDeBounce 25
const int chargeFor = 25;
const int numReadPass = 150;
const int maxWaitCnt=1000000;

int readCap(int numRead, int chargeCycles) {
  volatile int totWait=0;
  volatile int waitedFor=0;
  volatile int ar;
  for (int pn=0; pn &amp;lt; numRead; pn++) {
     // Wait for capacitor to Charge
	 GPIO_PinWrite(PIN_p28_GPIO , PIN_p28_PORT, PIN_p28_PIN, 1);
     volatile short posCnt=0;
     volatile int xx = 0;
     while((xx &amp;lt; chargeCycles) || (posCnt &amp;lt; posCntDeBounce)) {
    	xx++;
		ar = GPIO_PinRead(PIN_ACIN_GPIO, PIN_ACIN_PORT,PIN_ACIN_PIN);
		if (ar == 1) {
			posCnt++;
		} else  {
			posCnt--;
		}
     }

	 waitedFor=0;
	 // Set our Drain Pin to drain mode drawing power off the
	 // capacitor until it crosses Logic-0 threshold.
	 GPIO_PinWrite(PIN_p28_GPIO , PIN_p28_PORT, PIN_p28_PIN, 0);
	 volatile short negCnt=0;
	 while((waitedFor &amp;lt; maxWaitCnt)) {
		waitedFor++;
		ar = GPIO_PinRead(PIN_ACIN_GPIO, PIN_ACIN_PORT,PIN_ACIN_PIN);
		if (ar == 0) {
			negCnt++;
			if (negCnt &amp;gt; negCntDeBounce) {
				break;
			}
		} else {
			negCnt--;
		}
	 }
	 totWait += waitedFor;
  }

  return (( totWait * 100) /  numRead) -  (negCntDeBounce * 100);
}

#ifdef PRINTDELAY
#define PRINTEVERY 50000
#else
#define PRINTEVERY 0
#endif

/*
 * @brief   Application entry point.
 */
int main(void) {

    /* Init board hardware. */
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
    /* Init FSL debug console. */
    BOARD_InitDebugConsole();
#endif


    PRINTF("LCP804 Capacitance Test\n");
    GPIO_PinWrite(PIN_LED_GPIO , PIN_LED_PORT, PIN_LED_PIN, 0);

	volatile int x=0;
    /* Enter an infinite loop, just incrementing a counter. */
    while(1) {
	   x++;
	   if (x &amp;gt; PRINTEVERY) {
		  x = 0;
		  GPIO_PinWrite(PIN_LED_GPIO , PIN_LED_PORT, PIN_LED_PIN, 1);
		  int capr = readCap(numReadPass, chargeFor);
		  #ifdef PRINTDELAY
		     PRINTF("%d\n", capr);
          #endif
		  GPIO_PinWrite(PIN_LED_GPIO , PIN_LED_PORT, PIN_LED_PIN, 0);

	   }
       /* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
        __asm volatile ("nop");
    }
    return 0 ;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After increasing scale of returned number from over sampling by a factor of 100 it largely solved my concerns about sensitivity and I can now see material reading increases as my hand approaches the sensor solenoid starting at about 6" away.&amp;nbsp; &amp;nbsp;Still not as sensitive as what I am seeing out of 240Mhtz CPU but usable for a lot less power.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 11 May 2024 19:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863701#M56010</guid>
      <dc:creator>joeatrainamp</dc:creator>
      <dc:date>2024-05-11T19:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: A C Example for measuring sub 2pF capacitance change using a LPC804 chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863807#M56012</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Q1)What is process to get an example like this added to the examples in the SDK?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;There is example in SDK, pls go to the directory:&lt;/P&gt;
&lt;P&gt;C:\nxp\MCUXpressoIDE_11.8.0_1165;&lt;/P&gt;
&lt;P&gt;open the MCUXPresso_IDE_UserGuide.pdf and check the Chapter 6 6. Importing Example Projects (from installed SDKs)&lt;/P&gt;
&lt;P&gt;Q2)What is best way to learn to port this to use the PLU instead of explicit C Code?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;The PLU module function is the same as PLD or FPGA, which can implement the combination or sequential(has 4 D flip-flop) circuit, I do not think your application needs it.&lt;/P&gt;
&lt;P&gt;Q3)What is the best process for sharing content like this with other LPC users?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&lt;/P&gt;
&lt;P&gt;Q4)Is it worth porting to use Analog comparator rather than gate logic transition threshold? What benefit will we likely gain?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;I suppose that gate logic transition threshold is gate by gate, chip by chip, but the ACMP has fixed threshold.&lt;/P&gt;
&lt;P&gt;Q5)Does anybody see a way to increase true resolution by a factor of 10 with clever circuit changes. This would allow either less jitter or less oversampling both of which could save power.&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;If the capacitance varies&amp;nbsp; 1% with the full water level range, it is a difficult work.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Sat, 11 May 2024 06:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863807#M56012</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-05-11T06:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: A C Example for measuring sub 2pF capacitance change using a LPC804 chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863877#M56015</link>
      <description>&lt;P&gt;Your answer for Q1 doesn't answer my question.&amp;nbsp; &amp;nbsp;I want to know the process to submit content so it can be made available to other users as sample code when they download the SDK.&lt;/P&gt;</description>
      <pubDate>Sat, 11 May 2024 19:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863877#M56015</guid>
      <dc:creator>joeatrainamp</dc:creator>
      <dc:date>2024-05-11T19:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: A C Example for measuring sub 2pF capacitance change using a LPC804 chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863993#M56017</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;At the time being, SDK is developed by NXP dedicated software team, there is not any channel for external user code to be embedded in SDK package.&lt;/P&gt;
&lt;P&gt;If you have recommendation to add code for a general application field, you can submit request, I can submit it to SDK team.&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 03:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/A-C-Example-for-measuring-sub-2pF-capacitance-change-using-a/m-p/1863993#M56017</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-05-13T03:42:55Z</dc:date>
    </item>
  </channel>
</rss>