<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Protocols: SPI,I2C,UART in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Protocols-SPI-I2C-UART/m-p/1863865#M56013</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;What is the speeds of protocols&amp;nbsp;SPI,I2C &amp;amp; UART in LPC55S16?&lt;/P&gt;&lt;P&gt;And which will be the suitable protocol to communicate Two microcontrollers between each other?&lt;/P&gt;</description>
    <pubDate>Sat, 11 May 2024 12:03:09 GMT</pubDate>
    <dc:creator>DHARSAN</dc:creator>
    <dc:date>2024-05-11T12:03:09Z</dc:date>
    <item>
      <title>Protocols: SPI,I2C,UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Protocols-SPI-I2C-UART/m-p/1863865#M56013</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;What is the speeds of protocols&amp;nbsp;SPI,I2C &amp;amp; UART in LPC55S16?&lt;/P&gt;&lt;P&gt;And which will be the suitable protocol to communicate Two microcontrollers between each other?&lt;/P&gt;</description>
      <pubDate>Sat, 11 May 2024 12:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Protocols-SPI-I2C-UART/m-p/1863865#M56013</guid>
      <dc:creator>DHARSAN</dc:creator>
      <dc:date>2024-05-11T12:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: Protocols: SPI,I2C,UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Protocols-SPI-I2C-UART/m-p/1880237#M56189</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227782"&gt;@DHARSAN&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. About the speeds of protocols SPI,I2C &amp;amp; UART in LPC55S16.&lt;/P&gt;&lt;P&gt;You can refer to LPC551x DATA SHEET 7.24.3&lt;/P&gt;&lt;P&gt;I2C&lt;/P&gt;&lt;P&gt;• Support standard, Fast-mode, and Fast-mode Plus (specific I2C pins) with data rates&lt;BR /&gt;of up to 1 Mbit/s.&lt;BR /&gt;• Support high-speed slave mode with data rates of up to 3.4 Mbit/s (specific I2C pins)&lt;/P&gt;&lt;P&gt;SPI&lt;/P&gt;&lt;P&gt;• Maximum supported bit rate for SPI master mode (transmit/receive) is 32 Mbit/s. The&lt;BR /&gt;maximum supported bit rate for SPI slave receive mode is 25 Mbit/s and for SPI slave&lt;BR /&gt;transmit mode is 16 Mbits/s.&lt;/P&gt;&lt;P&gt;UART&lt;/P&gt;&lt;P&gt;• Maximum bit rates of 10 Mbit/s in asynchronous mode and 25 Mbit/s in synchronous mode for USART functions.&lt;/P&gt;&lt;P&gt;2. Usually, UART is used for communication between two microcontrollers.&lt;/P&gt;&lt;P&gt;Hope this will help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jun 2024 03:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Protocols-SPI-I2C-UART/m-p/1880237#M56189</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-04T03:10:52Z</dc:date>
    </item>
  </channel>
</rss>