<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1788 ethernet wakeup in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522965#M5601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Thu Feb 04 01:45:01 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i was getting packets in wireshark, which i had send through LPC1788,but not getting TX_Done interrupt. getting receive done interrupts and wireshark received packets directly come to LPC1788. But i am not satisfied with this is this seems configuration part was successully done or i did any mistakes? why TX_Done is not comming? is it because of SA0,SA1,SA2 registers MAC address setting in wrong way? And is there any way to communicate through IP addresses?? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:59:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:59:43Z</dc:date>
    <item>
      <title>LPC1788 ethernet wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522962#M5598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Tue Feb 02 00:03:19 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i am using uezgui-1788-70wvm kit, i want to test ethernet with example provided by uez source code. For PHY connection which tools we have to use? i am new to communicate through MAC address. I found wireshark tool, this is only for receiving (i thought) or is there any transmit option??&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Very 1st time we have to send magic frame to our module(LAN8720 through RJ45) for wake-up right? If is it right then how can we send? Means which tools i have to use??&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; OR it can communicate first time after initialization&amp;nbsp; when LPC1788 send data to wireshark?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522962#M5598</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 ethernet wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522963#M5599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Wed Feb 03 01:33:02 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; With LPC1788 + LAN8720, we have to communicate using MAC id only or we can communicate with IP address also? I have probe using CRO and checked all ENET connections. some data is going through TXD0,TXD1,RXD0,RXD1. but in code nothing is happening means no interrupts was generated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Another thing i was observed is ENET registers map address starts from 0x20084000. when i power enable ENET in PCONP register,ENET registers contained total memory is filled with 0xaaaaaaaa(observed in memory browser). Means is any other thing was disturbing ENET?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;but if i write into registers and read at that time its values are valid. But main problem is how do i know initialization part is successfully done?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; i saw magic packet in reference manual of lpc1788, Is magic packet was send from device(LAN8720) to host or host must be send magic packet to device?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; please anyone clarify me, i really confusing mac address part also in some example they provided &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/* Ethernet MAC address to use (default). */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define emacMACADDR0&amp;nbsp;&amp;nbsp; 0x00&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define emacMACADDR1&amp;nbsp;&amp;nbsp; 0xBD &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define emacMACADDR2&amp;nbsp;&amp;nbsp; 0x33 &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define emacMACADDR3&amp;nbsp;&amp;nbsp; 0x06 &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define emacMACADDR4&amp;nbsp;&amp;nbsp; 0x68 &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define emacMACADDR5&amp;nbsp;&amp;nbsp; 0x22&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; iMACAddress[0] = emacMACADDR0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; iMACAddress[1] = emacMACADDR1;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; iMACAddress[2] = emacMACADDR2;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; iMACAddress[3] = emacMACADDR3;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; iMACAddress[4] = emacMACADDR4;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; iMACAddress[5] = emacMACADDR5;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;state-----------------------------------------1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_EMAC-&amp;gt;SA0 = (p-&amp;gt;iSettings.iMACAddress[5] &amp;lt;&amp;lt; 8)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | p-&amp;gt;iSettings.iMACAddress[4];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_EMAC-&amp;gt;SA1 = (p-&amp;gt;iSettings.iMACAddress[3] &amp;lt;&amp;lt; 8)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | p-&amp;gt;iSettings.iMACAddress[2];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_EMAC-&amp;gt;SA2 = (p-&amp;gt;iSettings.iMACAddress[1] &amp;lt;&amp;lt; 8)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | p-&amp;gt;iSettings.iMACAddress[0];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;state--------------------------------------------------2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But in document (UM10470.pdf) they mentioned &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SA0[15:8] = 1st octet&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SA0[7:0] = 2nd octet, etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if these bothe statements are true then 1st octet is emacMACADDR5 right?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if we want to send packets to host our packet format is &amp;lt;des add&amp;gt; &amp;lt;src add&amp;gt;&amp;lt;opt VLAN&amp;gt;&amp;lt;len&amp;gt; &amp;lt;paylod&amp;gt;&amp;lt;FCS&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;destination address octet 1 is stating from lsb to msb (bit-0 to bit-7),so we have to re-frame MAC addresses right?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja m.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522963#M5599</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:59:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 ethernet wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522964#M5600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Wed Feb 03 21:45:56 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i am confusing with Memory allocation to RX descriptors and Tx descriptors. is that constant defaults provided by uez source code (uEZ_v2.06c_SourceForge\uEZ_v2.06c_SourceForge\uEZ\Source\Processor\NXP\LPC17xx_40xx\LPC17xx_40xx_EMAC.c) are correct?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone explain me about these defaults. i was unable to understand these memory locations allcoation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja m.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522964#M5600</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 ethernet wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522965#M5601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Thu Feb 04 01:45:01 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i was getting packets in wireshark, which i had send through LPC1788,but not getting TX_Done interrupt. getting receive done interrupts and wireshark received packets directly come to LPC1788. But i am not satisfied with this is this seems configuration part was successully done or i did any mistakes? why TX_Done is not comming? is it because of SA0,SA1,SA2 registers MAC address setting in wrong way? And is there any way to communicate through IP addresses?? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522965#M5601</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 ethernet wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522966#M5602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Sat Feb 06 01:53:52 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; For debug purpose we have to connect Lan cable from RJ45 connector (which is connected to LAN8720) to hub? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or we can connect cross calbe through PC to LAN8720 of RJ45??&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i was connected cross cable from Kit to pc, but i didn't recognize the ip address of kit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;I reffered this link (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Flan8720a-issues" rel="nofollow" target="_blank"&gt;https://www.lpcware.com/content/forum/lan8720a-issues&lt;/A&gt;&lt;SPAN&gt;) i didn't even get any ip addresses and all as they mentioned in some wireshark screen shorts. That why i have doubt about this cross cable connection.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja m.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/522966#M5602</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 ethernet wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/1816226#M55504</link>
      <description>Although this thread looks way old, however for the sake of completeness. One can use Wake on LAN windows GUI utility to send magic packet to a device on a local network. You just need to register the device by entering its MAC address. &lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://apps.microsoft.com/detail/9nblggh51pb3?hl=en-us&amp;amp;gl=IN" target="_blank"&gt;https://apps.microsoft.com/detail/9nblggh51pb3?hl=en-us&amp;amp;gl=IN&lt;/A&gt;</description>
      <pubDate>Tue, 27 Feb 2024 06:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-ethernet-wakeup/m-p/1816226#M55504</guid>
      <dc:creator>gaurav_sharma</dc:creator>
      <dc:date>2024-02-27T06:48:18Z</dc:date>
    </item>
  </channel>
</rss>