<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC802 dev/evk board - where can I get the example application source code ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1862817#M56007</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to work through the source code of the example application that the LPC802 dev kit has pre-installed.&lt;/P&gt;&lt;P&gt;This is the app that reads the temperature sensor, potentiometer, etc and lights LED's in a face pattern.&lt;/P&gt;&lt;P&gt;This source code would seem to be an excellent starting point as it's interfacing with most peripherals on the board.&lt;/P&gt;&lt;P&gt;I have the SDK installed but it doesn't seem to contain the source code for this example app.&lt;/P&gt;&lt;P&gt;Internet searches refer to example bundles, but I can't find one for LPC802 dev board.&lt;/P&gt;&lt;P&gt;Where can I get the LPC802 dev/evk board example application source code ?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Fri, 10 May 2024 09:25:05 GMT</pubDate>
    <dc:creator>paulw2</dc:creator>
    <dc:date>2024-05-10T09:25:05Z</dc:date>
    <item>
      <title>LPC802 dev/evk board - where can I get the example application source code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1862817#M56007</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to work through the source code of the example application that the LPC802 dev kit has pre-installed.&lt;/P&gt;&lt;P&gt;This is the app that reads the temperature sensor, potentiometer, etc and lights LED's in a face pattern.&lt;/P&gt;&lt;P&gt;This source code would seem to be an excellent starting point as it's interfacing with most peripherals on the board.&lt;/P&gt;&lt;P&gt;I have the SDK installed but it doesn't seem to contain the source code for this example app.&lt;/P&gt;&lt;P&gt;Internet searches refer to example bundles, but I can't find one for LPC802 dev board.&lt;/P&gt;&lt;P&gt;Where can I get the LPC802 dev/evk board example application source code ?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Fri, 10 May 2024 09:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1862817#M56007</guid>
      <dc:creator>paulw2</dc:creator>
      <dc:date>2024-05-10T09:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802 dev/evk board - where can I get the example application source code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1879439#M56182</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187779"&gt;@paulw2&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The LPC802 dev/evk board example application source code is in&amp;nbsp;the attachment.&lt;/P&gt;
&lt;P&gt;Please kindly check it.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jun 2024 05:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1879439#M56182</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-03T05:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802 dev/evk board - where can I get the example application source code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1950026#M56823</link>
      <description>Hi Hang,&lt;BR /&gt;&lt;BR /&gt;Apologies for very late reply.&lt;BR /&gt;&lt;BR /&gt;Thank you very much for providing this.</description>
      <pubDate>Mon, 09 Sep 2024 10:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-dev-evk-board-where-can-I-get-the-example-application/m-p/1950026#M56823</guid>
      <dc:creator>paulw2</dc:creator>
      <dc:date>2024-09-09T10:58:23Z</dc:date>
    </item>
  </channel>
</rss>