<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC804 mcuXpresso Config ignoring Package Selection for LPC804M101JHI33 Package</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-mcuXpresso-Config-ignoring-Package-Selection-for/m-p/1862101#M55995</link>
    <description>&lt;P&gt;When using new project wizard I selected the LPC804M101JHI33 but what is always shown is the LPC804M101JDH24 in the package view.&amp;nbsp; &amp;nbsp;It also applies this in the Pin selection view.&amp;nbsp; &amp;nbsp;This causes issues with being able to assign correct pins to correct functions.&amp;nbsp; &amp;nbsp;I have also gone in through the project explorer and reselected the correct package but it does not change it for the tool.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;My Xpresso version is showing:&amp;nbsp;&amp;nbsp;MCUXpresso IDE v11.9.0 [Build 2144] [2024-01-05] and check for updates shows no updates found.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use&amp;nbsp; the stand along config tool downloaded yesterday I works correctly for&amp;nbsp;LPC804M101JHI33 However when I save the .MEX file and try to import it into a project in the full MCUXpresso I get a bunch of pin routing errors because it is working with an incorrect package and still will not act as if the&amp;nbsp;LPC804M101JHI33 was selected even after selecting the correct package from Project explorer.&lt;BR /&gt;&lt;BR /&gt;The same issue holds regardless of if the correct package is selected during the project create wizard or later during using the project explorer.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;When I close the workspace and reopen it recognizes issue with the message&amp;nbsp; attached and when I selected yes I did switch to the correct package format and did allow the import of the saved .MEX file.&amp;nbsp; This seems like a weird way to have to work around the issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 09 May 2024 03:27:55 GMT</pubDate>
    <dc:creator>joeatrainamp</dc:creator>
    <dc:date>2024-05-09T03:27:55Z</dc:date>
    <item>
      <title>LPC804 mcuXpresso Config ignoring Package Selection for LPC804M101JHI33 Package</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-mcuXpresso-Config-ignoring-Package-Selection-for/m-p/1862101#M55995</link>
      <description>&lt;P&gt;When using new project wizard I selected the LPC804M101JHI33 but what is always shown is the LPC804M101JDH24 in the package view.&amp;nbsp; &amp;nbsp;It also applies this in the Pin selection view.&amp;nbsp; &amp;nbsp;This causes issues with being able to assign correct pins to correct functions.&amp;nbsp; &amp;nbsp;I have also gone in through the project explorer and reselected the correct package but it does not change it for the tool.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;My Xpresso version is showing:&amp;nbsp;&amp;nbsp;MCUXpresso IDE v11.9.0 [Build 2144] [2024-01-05] and check for updates shows no updates found.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use&amp;nbsp; the stand along config tool downloaded yesterday I works correctly for&amp;nbsp;LPC804M101JHI33 However when I save the .MEX file and try to import it into a project in the full MCUXpresso I get a bunch of pin routing errors because it is working with an incorrect package and still will not act as if the&amp;nbsp;LPC804M101JHI33 was selected even after selecting the correct package from Project explorer.&lt;BR /&gt;&lt;BR /&gt;The same issue holds regardless of if the correct package is selected during the project create wizard or later during using the project explorer.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;When I close the workspace and reopen it recognizes issue with the message&amp;nbsp; attached and when I selected yes I did switch to the correct package format and did allow the import of the saved .MEX file.&amp;nbsp; This seems like a weird way to have to work around the issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 09 May 2024 03:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-mcuXpresso-Config-ignoring-Package-Selection-for/m-p/1862101#M55995</guid>
      <dc:creator>joeatrainamp</dc:creator>
      <dc:date>2024-05-09T03:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC804 mcuXpresso Config ignoring Package Selection for LPC804M101JHI33 Package</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-mcuXpresso-Config-ignoring-Package-Selection-for/m-p/1864124#M56018</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232811"&gt;@joeatrainamp&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I can reproduce this issue, i will report this issue to out MCUXpresso IDE team.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 07:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-mcuXpresso-Config-ignoring-Package-Selection-for/m-p/1864124#M56018</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-05-13T07:10:32Z</dc:date>
    </item>
  </channel>
</rss>