<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC54608 Program crash problem</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Program-crash-problem/m-p/1845696#M55849</link>
    <description>&lt;P&gt;Hello, may I ask, LPC54608 product in the client application of the program crash, but re-use IAP burned and returned to normal what is the cause?&lt;/P&gt;</description>
    <pubDate>Fri, 12 Apr 2024 02:58:43 GMT</pubDate>
    <dc:creator>Zhaozhiling</dc:creator>
    <dc:date>2024-04-12T02:58:43Z</dc:date>
    <item>
      <title>LPC54608 Program crash problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Program-crash-problem/m-p/1845696#M55849</link>
      <description>&lt;P&gt;Hello, may I ask, LPC54608 product in the client application of the program crash, but re-use IAP burned and returned to normal what is the cause?&lt;/P&gt;</description>
      <pubDate>Fri, 12 Apr 2024 02:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Program-crash-problem/m-p/1845696#M55849</guid>
      <dc:creator>Zhaozhiling</dc:creator>
      <dc:date>2024-04-12T02:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 Program crash problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Program-crash-problem/m-p/1845920#M55853</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suggest that you use IAP function to erase/program on-chip flash, because the IAP function executes code in internal RAM and operate flash. as you know when you operate the flash, the flash can not be accessed/executed from.&lt;/P&gt;
&lt;P&gt;If you write register to erase/program flash without using IAP function, So you have to disable all interrupt so that the flash is not accessed, furthermore, I suggest you copy the code to erase/program flash to internal SRAM and execute the code in SRAM to operate the flash.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Apr 2024 07:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Program-crash-problem/m-p/1845920#M55853</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-12T07:56:52Z</dc:date>
    </item>
  </channel>
</rss>