<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Rollback problem with SBL on LPC55S69</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833714#M55718</link>
    <description>&lt;P&gt;Yes my problem is with SD Card OTA mode with SFW&lt;/P&gt;</description>
    <pubDate>Fri, 22 Mar 2024 11:30:55 GMT</pubDate>
    <dc:creator>Kentinos</dc:creator>
    <dc:date>2024-03-22T11:30:55Z</dc:date>
    <item>
      <title>Rollback problem with SBL on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833005#M55709</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I am testing the secondary bootloader MCUBoot on the LPC55S69.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;For that, I followed the documentation MCUOTASBLSFWUG.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In order to update the main application (SFW) I am using the "Local FOTA" with an SD-Card.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The update works well. I can generate a new image, sign it with imgtool.py and put it in the SD Card. The SFW detects the SD Card and puts the new program in the secondary slot.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;At the next reboot, the SBL swap primary and secondary slots and boot on the primary slot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In order to test the rollback mechanism, I modified some bytes of the new signed image and put the corrupted image in the SD Card.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;The SFW puts the new program in the secondary slot, and at the next reboot, the SBL swaps the two slots. As the binary is corrupted, SBL doesn't boot it. However,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;the SBL doesn't rollback to use the correct image of the secondary slot. So, the board doesn't boot anymore.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does anyone know why? All help is welcome. Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My setup is the following:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;Last version of SBL and SFW availables on Github.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;SBL and SFW code not modified.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Toolchain : arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-eabi.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Parameters to generate the signed image with imgtool.py : python imgtool.py sign --key sign-rsa2048-priv.pem --encrypt enc-rsa2048-pub.pem --align 4 --version "1.3" --header-size 0x400 --pad-header --slot-size 0x30000 --max-sectors 32 sfw.bin sfw_signed.bin&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;Config of SBL and MCUBoot:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;Enable single image function : disabled&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Signing with RSA&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;MCUBOOT_SWAP_USING_MOVE 1&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;MCUBOOT_IMAGE_NUMBER 1&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;Config of SFW:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;Enable sfw standalone xip : disabled&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Enable from OTA&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;OTA from SD Card&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;OTA from u-disk : disabled&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;Here are the logs of the update:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;Bootloader Version 1.1.0

Primary image: magic=good, swap_type=0x2, copy_done=0x3, image_ok=0x1

Secondary image: magic=bad, swap_type=0x0, copy_done=0x2, image_ok=0x2

Boot source: primary slot

writing copy_done; fa_id=1 off=0xlx (0xlx)

Bootloader chainload address offset: 0x20000

Reset_Handler address offset: 0x20400

Jumping to the image



hello sfw.

Current image verison: 1.3.0

SD Card updating task enable.

Hello world1.

Hello world2.

Please insert a sd card into board.

Update done, the last update type: SD Card

Write OK flag: off = 0x4fe00

Hello world1.

Hello world2.

Card inserted.

Hello world1.

Hello world2.

reading...

new img verison: 1.4.0

updating...

finished

write update type = 0x1

write magic number offset = 0x7fe00

Please remove the SD Card!

sys rst...

Hello world1.

Hello world2.



hello sbl.

Bootloader Version 1.1.0

Primary image: magic=good, swap_type=0x2, copy_done=0x3, image_ok=0x1

Secondary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x3

Boot source: none

Swap type: test

erasing trailer; fa_id=1

initializing status; fa_id=1

writing swap_info; fa_id=1 off=0xlx (0xlx), swap_type=0x2ffd8 image_num=0x4ffd8

writing swap_size; fa_id=1 off=0xlx (0xlx)

writing magic; fa_id=1 off=0xlx (0xlx)

erasing trailer; fa_id=2

writing copy_done; fa_id=1 off=0xlx (0xlx)

Signature verification failed, Image in the primary slot is not valid!



hello sbl.

Bootloader Version 1.1.0

Primary image: magic=good, swap_type=0x2, copy_done=0x1, image_ok=0x2

Secondary image: magic=bad, swap_type=0x0, copy_done=0x2, image_ok=0x2

Boot source: none

Swap type: none

Signature verification failed, Image in the primary slot is not valid!&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 13:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833005#M55709</guid>
      <dc:creator>Kentinos</dc:creator>
      <dc:date>2024-03-21T13:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: Rollback problem with SBL on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833699#M55717</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231271"&gt;@Kentinos&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How about refer to "U-Disk and SD Card Update in SFW"&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13499.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN13499.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 22 Mar 2024 11:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833699#M55717</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-03-22T11:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: Rollback problem with SBL on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833714#M55718</link>
      <description>&lt;P&gt;Yes my problem is with SD Card OTA mode with SFW&lt;/P&gt;</description>
      <pubDate>Fri, 22 Mar 2024 11:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Rollback-problem-with-SBL-on-LPC55S69/m-p/1833714#M55718</guid>
      <dc:creator>Kentinos</dc:creator>
      <dc:date>2024-03-22T11:30:55Z</dc:date>
    </item>
  </channel>
</rss>