<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1788 CAN transmit interrupt</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-CAN-transmit-interrupt/m-p/522935#M5571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by r2djoe on Wed Nov 14 04:40:19 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to asynchronously send frames, so that the send method only needs to add the frame to a circular buffer, then the IRQ will figure out which TX buffer is free, and send the frame. I cannot find any documentation or examples on how to do this, or on the structure of the CAN_1-&amp;gt;ICR field. Any help would be appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:58:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:58:04Z</dc:date>
    <item>
      <title>LPC1788 CAN transmit interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-CAN-transmit-interrupt/m-p/522935#M5571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by r2djoe on Wed Nov 14 04:40:19 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to asynchronously send frames, so that the send method only needs to add the frame to a circular buffer, then the IRQ will figure out which TX buffer is free, and send the frame. I cannot find any documentation or examples on how to do this, or on the structure of the CAN_1-&amp;gt;ICR field. Any help would be appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-CAN-transmit-interrupt/m-p/522935#M5571</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:58:04Z</dc:date>
    </item>
  </channel>
</rss>