<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S16 SPI Communication issue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-Communication-issue/m-p/1829849#M55679</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that the SPI is in master mode, in the case, the MOSI, /CS and SCK are output signals. while the /CS(chip select) is high, I suppose that the MOSI is float, because there is not data transfer during the time, it does matter whether the MOSI is high or low. When the /CS is low, the MOSI pin is driven by master, it represents the data with the SCK.&lt;/P&gt;
&lt;P&gt;If you want the MOSI signal is high when the /CS is high, I suppose you can try to connect a 10K ohm pull-up resistor on the MOSI pin, pls have a try.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 18 Mar 2024 02:27:19 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-03-18T02:27:19Z</dc:date>
    <item>
      <title>LPC55S16 SPI Communication issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-Communication-issue/m-p/1829595#M55674</link>
      <description>&lt;P&gt;hello i've modified the library to use the spi with gpio pins but im unable to get communication. after probing the bus i noticed that the&amp;nbsp;Mosi line idles lows and our select Is triggering before the Mosi rises to begin transmission.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jmorel_0-1710529526921.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268744i9D7611CB67DAE18E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jmorel_0-1710529526921.png" alt="jmorel_0-1710529526921.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;is there a way to set the Mosi to idle high instead of low or is there a flag that is set to tell me when the transmission is going to begin i.e. once the Mosi exits idle.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 19:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-Communication-issue/m-p/1829595#M55674</guid>
      <dc:creator>jmorel</dc:creator>
      <dc:date>2024-03-15T19:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 SPI Communication issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-Communication-issue/m-p/1829849#M55679</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that the SPI is in master mode, in the case, the MOSI, /CS and SCK are output signals. while the /CS(chip select) is high, I suppose that the MOSI is float, because there is not data transfer during the time, it does matter whether the MOSI is high or low. When the /CS is low, the MOSI pin is driven by master, it represents the data with the SCK.&lt;/P&gt;
&lt;P&gt;If you want the MOSI signal is high when the /CS is high, I suppose you can try to connect a 10K ohm pull-up resistor on the MOSI pin, pls have a try.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 02:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-Communication-issue/m-p/1829849#M55679</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-03-18T02:27:19Z</dc:date>
    </item>
  </channel>
</rss>