<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S14 Assembly Programming on Keil</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1825897#M55622</link>
    <description>&lt;P&gt;Thanks for the info.&lt;/P&gt;</description>
    <pubDate>Tue, 12 Mar 2024 08:10:57 GMT</pubDate>
    <dc:creator>PBrunay</dc:creator>
    <dc:date>2024-03-12T08:10:57Z</dc:date>
    <item>
      <title>LPC55S14 Assembly Programming on Keil</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1802388#M55353</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I got an interest on LPC55S14 Microcontroller. I'm using keil uvision 5 IDE. I would like to try programming this chip using assembly language. Can I have a sample startup file and a simple main file just to begin with?&lt;/P&gt;&lt;P&gt;By the way, I'm already familiar with arm cortex m3/m4 instructions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 06:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1802388#M55353</guid>
      <dc:creator>PBrunay</dc:creator>
      <dc:date>2024-02-06T06:34:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S14 Assembly Programming on Keil</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1802615#M55357</link>
      <description>&lt;P&gt;I would say, the best place to ask would be the Keil forum.&lt;/P&gt;&lt;P&gt;But AFAIK, the Keil startup file (as with most toolchains) comes already as assembler code.&lt;BR /&gt;For the "main" file, you could start out from a basic C project, and review the generated assembler code.&lt;BR /&gt;Not sure if the Keil IDE has a project wizard for assember-based projects, but you can always add assember files to a C project.&lt;/P&gt;&lt;P&gt;Two notes:&lt;BR /&gt;The Arm/Keil assembly file syntax used to differ slightly from the GCC toolchain syntax. I think this is still the case.&lt;BR /&gt;And second, you might need to explicitely enable the generation of assembly ("intermediate") files in the project settings, many toolchains don't do that by default any more.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 11:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1802615#M55357</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2024-02-06T11:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S14 Assembly Programming on Keil</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1825897#M55622</link>
      <description>&lt;P&gt;Thanks for the info.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 08:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S14-Assembly-Programming-on-Keil/m-p/1825897#M55622</guid>
      <dc:creator>PBrunay</dc:creator>
      <dc:date>2024-03-12T08:10:57Z</dc:date>
    </item>
  </channel>
</rss>