<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Source code erased from flash after power cycle on LPC5506</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820567#M55553</link>
    <description>I'm sorry for the misunderstood, i mean BootROM.&lt;BR /&gt;I cannot retrieve the schematic but is strange that flash perform like ram... there is some configuration to check into the project settings in MCUXpresso?</description>
    <pubDate>Mon, 04 Mar 2024 13:22:35 GMT</pubDate>
    <dc:creator>WorkerEmbedded</dc:creator>
    <dc:date>2024-03-04T13:22:35Z</dc:date>
    <item>
      <title>Source code erased from flash after power cycle on LPC5506</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1818624#M55524</link>
      <description>&lt;P&gt;Hi everybody, i've got a huge problem!&lt;/P&gt;&lt;P&gt;Previously, i've developed a project which involped LPC55S69-EVK and OM-SE05ARD-E.&lt;/P&gt;&lt;P&gt;Everything seemsed to be alright and i started to make porting to a custom PCB developed with a LPC5506.&lt;/P&gt;&lt;P&gt;The porting works, the I2C with Secure element is going well and all the periphals are working good.&lt;/P&gt;&lt;P&gt;There is an issue, when i perform a power cycle (power off-on) all the data saved in flash are erased and it's like i've never upload the firmware inside the MCU.&lt;/P&gt;&lt;P&gt;The flash was set correctly (starting from 0x00000000), even the RAM (starting from 0x20000000) in according to the documentation.&lt;/P&gt;&lt;P&gt;I don't undertand if is an ISP problem (via hardware).&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 09:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1818624#M55524</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2024-02-29T09:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: Source code erased from flash after power cycle on LPC5506</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1819321#M55535</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224071"&gt;@WorkerEmbedded&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How about just program a simple demo, like led? Then&amp;nbsp;&lt;SPAN&gt;perform a power cycle, check whether flash are erased?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 07:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1819321#M55535</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-03-01T07:08:22Z</dc:date>
    </item>
    <item>
      <title>Re: Source code erased from flash after power cycle on LPC5506</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820261#M55545</link>
      <description>&lt;P&gt;Yes, i've already tried but nothin, same result.&lt;/P&gt;&lt;P&gt;This are the log:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;[...]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Content of CoreSight Debug ROM(s):&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;RBASE E00FE000: CID B105100D PID 0000095000 ROM (type 0x1)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;ROM 1 E00FF000: CID B105100D PID 04000BB4C9 ROM (type 0x1)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;ROM 2 E000E000: CID B105900D PID 04000BBD21 CSt ARM ARMv8-M type 0x0 Misc - Undefined&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;ROM 2 E0001000: CID B105900D PID 04000BBD21 CSt ARM DWTv2 type 0x0 Misc - Undefined&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;ROM 2 E0002000: CID B105900D PID 04000BBD21 CSt ARM FPBv2 type 0x0 Misc - Undefined&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;ROM 2 E0000000: CID B105900D PID 04000BBD21 CSt ARM ITMv2 type 0x43 Trace Source - Bus&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;ROM 1 E0040000: CID B105900D PID 04000BBD21 CSt type 0x11 Trace Sink - TPIU&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;NXP: LPC5506&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;DAP stride is 1024 bytes (256 words)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Inspected v.2 On chip Flash memory using IAP lib LPC550x.cfx&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Image 'LPC550x Dec 12 2023 17:11:31'&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Opening flash driver LPC550x.cfx&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;VECTRESET requested, but not supported on ARMv8-M CPUs. Using SOFTRESET instead.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Using SOFT reset to run the flash driver&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Flash variant 'LPC550x (244KB)' detected (244KB = 488*512 at 0x0)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Closing flash driver LPC550x.cfx&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Connected: was_reset=true. was_stopped=false&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Awaiting telnet connection to port 3330 ...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;GDB nonstop mode enabled&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Opening flash driver LPC550x.cfx (already resident)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;VECTRESET requested, but not supported on ARMv8-M CPUs. Using SOFTRESET instead.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Using SOFT reset to run the flash driver&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Flash variant 'LPC550x (244KB)' detected (244KB = 488*512 at 0x0)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Writing 12708 bytes to address 0x00000000 in Flash&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Sectors written: 0, unchanged: 25, total: 25&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Erased/Wrote sector 0-24 with 12708 bytes in 42msec&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Closing flash driver LPC550x.cfx&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Flash Write Done&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Flash Program Summary: 12708 bytes in 0.04 seconds (295.48 KB/sec)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Starting execution using system reset and halt target with a stall address&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;Retask read watchpoint 1 at 0x50000040 to use for boot ROM stall&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808000"&gt;&lt;SPAN&gt;Warning - processor did not halt - gave up waiting&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;flash - system reset failed - Ep(04). Cannot halt processor.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;Target error from Commit Flash write: Ep(04). Cannot halt processor.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808000"&gt;&lt;SPAN&gt;GDB stub (C:\nxp\LinkServer_1.4.85\binaries\crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#808080"&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I've already tried to modify reset handling in debug configuration, the demo start but is not persistent in flash and the bootloader cannot upload it after a power cycle&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 04 Mar 2024 07:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820261#M55545</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2024-03-04T07:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: Source code erased from flash after power cycle on LPC5506</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820521#M55549</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224071"&gt;@WorkerEmbedded&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;the bootloader cannot upload it after a power cycle&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; The bootloader mean BOOT ROM or your own second bootloader?&lt;/P&gt;
&lt;P&gt;How about refer to schematic to check your hardware?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 12:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820521#M55549</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-03-04T12:00:38Z</dc:date>
    </item>
    <item>
      <title>Re: Source code erased from flash after power cycle on LPC5506</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820567#M55553</link>
      <description>I'm sorry for the misunderstood, i mean BootROM.&lt;BR /&gt;I cannot retrieve the schematic but is strange that flash perform like ram... there is some configuration to check into the project settings in MCUXpresso?</description>
      <pubDate>Mon, 04 Mar 2024 13:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1820567#M55553</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2024-03-04T13:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: Source code erased from flash after power cycle on LPC5506</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1821964#M55571</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224071"&gt;@WorkerEmbedded&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can check memory detail as below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1709690177794.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266678iB1F4E85FD9711DF9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1709690177794.png" alt="Alice_Yang_0-1709690177794.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1709690177794.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Or linker files and .map file:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_1-1709690242372.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266680i350683F2386E2F62/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_1-1709690242372.png" alt="Alice_Yang_1-1709690242372.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_1-1709690242372.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;While, if you use SDK demo, the default memory is Flash.&lt;/P&gt;
&lt;P&gt;Also please check the part number&amp;nbsp; in project is the same with your chip.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 01:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Source-code-erased-from-flash-after-power-cycle-on-LPC5506/m-p/1821964#M55571</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-03-06T01:58:46Z</dc:date>
    </item>
  </channel>
</rss>