<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using LPC1788FBD208K for a new design with a 7&amp;quot; TFT in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC1788FBD208K-for-a-new-design-with-a-7-quot-TFT/m-p/1818876#M55527</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm integrating an LPC1788FBD208K into a new product. I'll use the MCU to directly control a 7" TFT LCD screen with a 24-bit RGB interface. I can see that the MCU does have a specialized module for TFT screen control, but I haven't been able to find any tool that allows me to design GUIs easily. I searched through the GUI Guider documentation, but it seems it's not compatible with the MCU I want to use. Do you have any tools I could use to create the GUI more easily? I really wouldn't want to have to program all the graphical windows myself, and I might even consider using another MCU that has a TFT LCD controller module if necessary to use GUI Guider or LVGL with MCUXpresso SDK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Walter.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Feb 2024 16:24:54 GMT</pubDate>
    <dc:creator>MartinEnG</dc:creator>
    <dc:date>2024-02-29T16:24:54Z</dc:date>
    <item>
      <title>Using LPC1788FBD208K for a new design with a 7" TFT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC1788FBD208K-for-a-new-design-with-a-7-quot-TFT/m-p/1818876#M55527</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm integrating an LPC1788FBD208K into a new product. I'll use the MCU to directly control a 7" TFT LCD screen with a 24-bit RGB interface. I can see that the MCU does have a specialized module for TFT screen control, but I haven't been able to find any tool that allows me to design GUIs easily. I searched through the GUI Guider documentation, but it seems it's not compatible with the MCU I want to use. Do you have any tools I could use to create the GUI more easily? I really wouldn't want to have to program all the graphical windows myself, and I might even consider using another MCU that has a TFT LCD controller module if necessary to use GUI Guider or LVGL with MCUXpresso SDK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Walter.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 16:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC1788FBD208K-for-a-new-design-with-a-7-quot-TFT/m-p/1818876#M55527</guid>
      <dc:creator>MartinEnG</dc:creator>
      <dc:date>2024-02-29T16:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPC1788FBD208K for a new design with a 7" TFT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC1788FBD208K-for-a-new-design-with-a-7-quot-TFT/m-p/1819142#M55532</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LPC1788 is a bit old, it was launched in 2013 year.&lt;/P&gt;
&lt;P&gt;The GUI guider does not support the LPC1788, if you want to use GUI guider tools to develop graphic interface, I suggest you consider LPC54xxx including LPC54628, LPC54018 which have LCD interface and GUI guider supports the two chips.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 02:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC1788FBD208K-for-a-new-design-with-a-7-quot-TFT/m-p/1819142#M55532</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-03-01T02:41:49Z</dc:date>
    </item>
  </channel>
</rss>