<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC824 recommended quartz oscillator</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-recommended-quartz-oscillator/m-p/1817569#M55515</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am looking for a quartz oscillator to be used with the LPC824. I have seen that the LPCXpresso824-MAX Board uses the&amp;nbsp;ABLS2-12.000MHZ-D4Y-T but it is too bluky for my new board (about 10mm length). Is there anything else with smaller footprint that you can recommend? Is ABM3B-12.000MHZ-B2-T a good replacement?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Wed, 28 Feb 2024 15:00:33 GMT</pubDate>
    <dc:creator>topspin</dc:creator>
    <dc:date>2024-02-28T15:00:33Z</dc:date>
    <item>
      <title>LPC824 recommended quartz oscillator</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-recommended-quartz-oscillator/m-p/1817569#M55515</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am looking for a quartz oscillator to be used with the LPC824. I have seen that the LPCXpresso824-MAX Board uses the&amp;nbsp;ABLS2-12.000MHZ-D4Y-T but it is too bluky for my new board (about 10mm length). Is there anything else with smaller footprint that you can recommend? Is ABM3B-12.000MHZ-B2-T a good replacement?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 15:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-recommended-quartz-oscillator/m-p/1817569#M55515</guid>
      <dc:creator>topspin</dc:creator>
      <dc:date>2024-02-28T15:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 recommended quartz oscillator</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-recommended-quartz-oscillator/m-p/1818209#M55520</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think it is okay to use any 12MHz crystal with proper load capacitor.&lt;/P&gt;
&lt;P&gt;so the ABM3B-12.000MHZ-B2-T is okay, the load cap is 18pF, so the two capacitor value is:&lt;/P&gt;
&lt;P&gt;CX1=CX2=18pF*2=36pF.&lt;/P&gt;
&lt;P&gt;Considering the parasitic cap, you can use 33pF cap for the CX1 and CX2.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 02:17:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-recommended-quartz-oscillator/m-p/1818209#M55520</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-02-29T02:17:48Z</dc:date>
    </item>
  </channel>
</rss>