<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Replacement of SWM(Switch Matrix) in LPC55s69 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Replacement-of-SWM-Switch-Matrix-in-LPC55s69/m-p/1814384#M55491</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229839"&gt;@ravicha&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;USART functions are available on all LPC55S6x/LPC55S2x/LPC552x devices as a&lt;BR /&gt;selectable function in each Flexcomm Interface peripheral. Up to 8 Flexcomm Interfaces&lt;BR /&gt;are available. So you can choose two of them to use.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Fri, 23 Feb 2024 06:51:00 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2024-02-23T06:51:00Z</dc:date>
    <item>
      <title>Replacement of SWM(Switch Matrix) in LPC55s69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Replacement-of-SWM-Switch-Matrix-in-LPC55s69/m-p/1812806#M55481</link>
      <description>&lt;P&gt;i have code for LPC804 of UART1 and UART2 where UART1 is responsible for communication to the smart card and UART2 is for genrating the clock for smart card , this two UART used throught SWM&amp;nbsp;&lt;/P&gt;&lt;P&gt;now i want to replace this in lpc55s69 how to do it&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 12:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Replacement-of-SWM-Switch-Matrix-in-LPC55s69/m-p/1812806#M55481</guid>
      <dc:creator>ravicha</dc:creator>
      <dc:date>2024-02-21T12:16:27Z</dc:date>
    </item>
    <item>
      <title>Re: Replacement of SWM(Switch Matrix) in LPC55s69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Replacement-of-SWM-Switch-Matrix-in-LPC55s69/m-p/1814384#M55491</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229839"&gt;@ravicha&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;USART functions are available on all LPC55S6x/LPC55S2x/LPC552x devices as a&lt;BR /&gt;selectable function in each Flexcomm Interface peripheral. Up to 8 Flexcomm Interfaces&lt;BR /&gt;are available. So you can choose two of them to use.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 23 Feb 2024 06:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Replacement-of-SWM-Switch-Matrix-in-LPC55s69/m-p/1814384#M55491</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-02-23T06:51:00Z</dc:date>
    </item>
  </channel>
</rss>