<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC176x.h in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC176x-h/m-p/522904#M5540</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leluno on Sat Feb 08 04:47:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;i'm working with lpcxpresso and i'm very satisfyed. Thank you for this fine programm.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But there seems to be a problem with the CCR-Register. Which one? there are two:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Configuration and Control Register CCR 0xE000ED14&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Clock Control Register CCR 0x40024008&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this ok?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In LPC176x.h &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RxFliterCtrl must be named RxFilterCtrl&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MIN for minute of rtc makes Proplems because of MIN/MAX in other functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:58:31 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:58:31Z</dc:date>
    <item>
      <title>LPC176x.h</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC176x-h/m-p/522904#M5540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leluno on Sat Feb 08 04:47:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;i'm working with lpcxpresso and i'm very satisfyed. Thank you for this fine programm.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But there seems to be a problem with the CCR-Register. Which one? there are two:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Configuration and Control Register CCR 0xE000ED14&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Clock Control Register CCR 0x40024008&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this ok?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In LPC176x.h &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RxFliterCtrl must be named RxFilterCtrl&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MIN for minute of rtc makes Proplems because of MIN/MAX in other functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:58:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC176x-h/m-p/522904#M5540</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:58:31Z</dc:date>
    </item>
  </channel>
</rss>