<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Standalone LinkServer Problem while Flash Programming in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798554#M55288</link>
    <description>&lt;P&gt;Thank you so much. The makefile command that works for me at below.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/usr/local/LinkServer/LinkServer flash LPC802 load -e -a 0 ./build/Blink.bin&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jan 2024 09:39:03 GMT</pubDate>
    <dc:creator>BahadirA</dc:creator>
    <dc:date>2024-01-31T09:39:03Z</dc:date>
    <item>
      <title>Standalone LinkServer Problem while Flash Programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798354#M55282</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I want to programming LPC802 microcontroller with makefile and standalone LinkServer. Also Mcuxpresso is installed at my PC.&lt;/P&gt;&lt;P&gt;When I use MCUexpresso's &lt;STRONG&gt;crt_emu_cm_redlink &lt;/STRONG&gt;everything is fine, I can flash programming that makefile command at below.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt; /usr/local/mcuxpressoide-11.8.0_1165/ide/binaries/crt_emu_cm_redlink -pLPC802 -vendor=NXP -flash-load-exec "./build/Blink.bin" -load-base=0x00000000 &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when i use standalone LinkServer it's fail. Makefile command at error message at below.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/usr/local/LinkServer_1.4.85/binaries/crt_emu_cm_redlink -pLPC802 -vendor=NXP -flash-load-exec "./build/Blink.bin" -load-base=0x00000000 &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Ns: MCUXpresso IDE RedlinkMulti Driver v11.9 (Dec 11 2023 18:09:23 - crt_emu_cm_redlink build 2)
Wc(03). No cache support.
Nc: Didn't find chip 'LPC802' vendor 'NXP' in any part information directory
Ea: part information directories:
Ea: -x "/usr/local/LinkServer_1.4.85/binaries"
Nc: chip initialization failed - Ec(04). Chip name unknown in library.
Et:51: This MCU is not supported by the product (Failed on -p named Package (chip/board) lookup).
make: *** [Makefile:210: instalit] Error 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Only versions are different (11.9 &amp;amp; 11.8). How can i fix it ?&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 06:35:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798354#M55282</guid>
      <dc:creator>BahadirA</dc:creator>
      <dc:date>2024-01-31T06:35:39Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone LinkServer Problem while Flash Programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798373#M55284</link>
      <description>&lt;P&gt;I recommend that you are not using the crt_emu_cm_redlink, as there is a standalone linkserver package/installation available from NXP, which is intended to be used as such.&lt;/P&gt;&lt;P&gt;See &lt;A href="https://mcuoneclipse.com/2023/05/14/linkserver-for-microcontrollers/" target="_blank"&gt;https://mcuoneclipse.com/2023/05/14/linkserver-for-microcontrollers/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 06:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798373#M55284</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2024-01-31T06:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone LinkServer Problem while Flash Programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798554#M55288</link>
      <description>&lt;P&gt;Thank you so much. The makefile command that works for me at below.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/usr/local/LinkServer/LinkServer flash LPC802 load -e -a 0 ./build/Blink.bin&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 09:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Standalone-LinkServer-Problem-while-Flash-Programming/m-p/1798554#M55288</guid>
      <dc:creator>BahadirA</dc:creator>
      <dc:date>2024-01-31T09:39:03Z</dc:date>
    </item>
  </channel>
</rss>